Announcements

Industry-first USB 10Gbps device controller. Check it out now!

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

USB superspeed peripherals Forum Discussions

lopo_1264666
USB superspeed peripherals
I would like to define constant at fixed location for FX3 so that when I analyze the image file, I can read its value at this known address. From FX3 ... Show More
ThAl_4704151
USB superspeed peripherals
One of the first things I do in my program (after calling CyU3PDeviceInit() and CyU3PDeviceCacheControl()) is call CyU3PDeviceConfigureIOMatrix().I'm ... Show More
TeLu_4270821
USB superspeed peripherals
I am using FX3 implement a test, The transfer like below:PC(HOST) ←→ FX3 ← Async SRAM interface(80Mhz) → MCU(STM32)Here are what I did. Refer AN76405 ... Show More
shsa_4792201
USB superspeed peripherals
I2C EEPROM (AT24CM01) for boot is connected to Cyusb3014, PMODE is changed, and USB boot and I2C boot are used depending on the situation.I want to ch... Show More
DaGr_4328696
USB superspeed peripherals
I'm currently working on a project that sets up a UVC video stream using the FX3. When the device is plugged into a host directly, it works absolutely... Show More
ArSa_3842301
USB superspeed peripherals
Hi,I have developed an own PCB design based on Denebola development kit. Whit the following differences:-  the SPI FLASH, which is used to store the f... Show More
LuTa_4642501
USB superspeed peripherals
Hi, I need to use spritf with the demo cyfxusbdebug, but it doest compile::tanureal@archtower $ make make[1]: Entering directory '/media/workspace/usb... Show More
KaFu_3122371
USB superspeed peripherals
I would like confirmation of the behavior of a standalone DMA_RDY_TH* event within the transition equation of a GPIF II state machine. What I mean is ... Show More
ArSa_3842301
USB superspeed peripherals
Hello,According to the CX3 datasheet, the device can load boot images from varios sources. And it is necessary to adjust the configuration of the PMOD... Show More
ArSa_3842301
USB superspeed peripherals
Hello,I am carrying out an own design based on Denebola board. I know that is possible to store the boot image in both : into an SPI Flash memory or i... Show More
Forum Information

USB superspeed peripherals

Discussion forum regarding USB superspeed peripherals topics.