Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

USB superspeed peripherals Forum Discussions

Sort by:
Robin_Peng
USB superspeed peripherals

Dears

我们用USB3014做设计,想请教下可否将PAL输入默认是1280*720的改成(720*576)的?谢谢

DiDi_4439146
USB superspeed peripherals
I am testing with a couple examples from the FX3 SDK (namely the usb HID Mouse example). I modified the code slightly so that it will continuously sen... Show More
DiDi_4439146
USB superspeed peripherals
Hi I have a simple application on the FX3 which just turns an LED on, I then shut off my computer and the LED remains on. What should I do if I want t... Show More
LuCu_4098176
USB superspeed peripherals
Hello,I am using the slave fifo implementation provided with no code changes in what respects the slave fifo.(only added very little code to implement... Show More
GrHa_3282776
USB superspeed peripherals
Hi,I having problems specifying and sourcing a 52 Mhz CMOS oscillator at 3.3V for the CYUSB3014.  Is there a recommended PN?  And is there a reference... Show More
AlEr_4025481
USB superspeed peripherals
Hi there,I'm fighting with data lost during DMA transfer and totally stuck on two questions... To be sure that received data is monotonic I attached a... Show More
LuCu_4098176
USB superspeed peripherals
Hello,Sometimes after a manual hard reset (without powering off everything) the boot defaults to USB and the code stored in the eeprom is no longer re... Show More
liwe_284431
USB superspeed peripherals
Hello, I asked this question two years ago , Re: When usb3.1 Gen 2 FX3 chip will be released? Now is 2020 , I am still waiting for GEN2 Controller....... Show More
YuRe_4727406
USB superspeed peripherals
Hey guys, I'm trying to config a FPGA via SelectMap mode. And what I did is to use GPIO to emulate a 16-bit parallel IO. It works but the speed is qui... Show More
IyRa_4728991
USB superspeed peripherals
Hi All,I am new to USB environment. My aim is to port from windows to android to communicate with hardware peripheral using cypress device. Existing s... Show More
Forum Information

USB superspeed peripherals

Discussion forum regarding USB superspeed peripherals topics.