Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

USB superspeed peripherals Forum Discussions

USB superspeed peripherals Forum Discussions

Sort by:
OfOr_1738446
USB superspeed peripherals
c# video app
Solved
Hello,I wrote a C# application co interface with my Cypress FX3 camera.To see the video stream, i'm using Aforge and for the command I use the using C... Show More
adki_3154446
USB superspeed peripherals
Hi,we using the streamer SDK and we want to understand the meanings of the following failures  :we want to distinguish between the failure types that ... Show More
ElTa_4521156
USB superspeed peripherals
Hi,I connect my FX3 card to USB port, it shows FX3 in device type. after programming .img file, it recognize my device type as FX2 in cyusb_linux. why... Show More
zoho_1277946
USB superspeed peripherals
CY68013 uses the BulkInEndPt function to read the buffer. It seems that it can only read 512 bytes or more. For example, what should I do if I want to... Show More
TeLe_4638221
USB superspeed peripherals
Hi All,I am working cypress FX3. I changed clock setting in GPIF designer to internal clock. I just modified Clock settings in GPIF II Designer. and C... Show More
HaHu_4486526
USB superspeed peripherals
i try to set a GPIO as an input pin with pull-up internally in FX3. but it is failed. i don't know how to set GCTL_WPU_CFG register in firmware.who ca... Show More
Peya_4162826
USB superspeed peripherals
I would like to change USB mode between USB 2.0 and 3.0 base on SDK 1.3.4 demo module " cyfxbulklpmandcache" , but it cannot be successful.It always r... Show More
KeWa_2323766
USB superspeed peripherals
I use test host application provided in the following link. UVC Extension unit https://community.cypress.com/message/142801#142801I didn't change the ... Show More
NoAr_1540581
USB superspeed peripherals
HelloAsynchronous SRAM timing is used by using CYUSB3014. However, since tOHC is 0.5ns on the customer's system, the operation can not be guaranteed b... Show More
WGT_4383351
USB superspeed peripherals
Just tested the firmware, have some problem/question:(1) First, use control center to test the 16KB IN or OUT endpoint, but both have inifnite capacit... Show More
Forum Information

USB superspeed peripherals

Discussion forum regarding USB superspeed peripherals topics.