Hello, I'm looking for some technical info concerning your CYUSB3065 device. In the datasheet I see that the device is USB 2.0 compatible and I'd like to know if that means it can communicate over the USB2.0 D+/D- lines only and if there are any band width restrictions when used in the USB2.0 only mode.
Looking forward to hearing back
Solved! Go to Solution.
Hi Dan,
Thank you for contacting Infineon Developer Community.
CYUSB3065 is a superspeed (USB 3) peripheral controller used as a bridge between image sensor having MIPI interface and USB.
CYUSB3065 is USB 2 compatible. It means that the CYUSB3065 can also work as a highspeed (USB 2) device over the D+/D- lines.
When used in USB 2 only mode, the maximum throughput CYUSB3065 can provide is ~40MBps,
Make sure the video bandwidth for USB 2< 35-40MBps.
Best Regards,
AliAsgar
Hi Dan,
Thank you for contacting Infineon Developer Community.
CYUSB3065 is a superspeed (USB 3) peripheral controller used as a bridge between image sensor having MIPI interface and USB.
CYUSB3065 is USB 2 compatible. It means that the CYUSB3065 can also work as a highspeed (USB 2) device over the D+/D- lines.
When used in USB 2 only mode, the maximum throughput CYUSB3065 can provide is ~40MBps,
Make sure the video bandwidth for USB 2< 35-40MBps.
Best Regards,
AliAsgar