- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
HI,
USBBulkSOurceSink Streming example on CYUSB3KIT-003 stop blinking LED after reflash.
<DEVICE>
FriendlyName="Cypress FX3 USB StreamerExample Device"
Manufacturer="Cypress"
Product="FX3"
SerialNumber=""
Configurations="1"
MaxPacketSize="512"
VendorID="04 B4"
ProductID="00 F1"
Class="00h"
SubClass="00h"
Protocol="00h"
BcdDevice="00 00"
BcdUSB="03 10"It enumerates as
And Streaming test still gives more than 4 MBps (4-5 Gbps).
And trying to modify blink rate according to example gives:
CONTROL OUT transfer
CONTROL OUT transfer failed with Error Code:997
I can still send and receive data on Bulk In and Out endpoint.
The example BootLedBlink - blinks the diode.
What can be the issue?
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
OKAY - Issue solved.
Actually there are two sw packages to be intalled: The one mentioned in the KIT, AND the 'old' one: The "SuperSpeed Explorer Kit". It is this the UG addresses. The FW example under the "SuperSpeed Explorer Kit" works.