Hi: I used the solution provided by this link. After download the img, two FX3 unknown devices appears in device manager.
But when I update the driver , pop the message" i can't find the driver".
Is the program is tested?
Hi,
Are you using AN75779? If you want to add CDC interface to UVC application?
No.I use slaveFifoSync(AN65974).
I dowanload the SlaveFifoSync.rar file from the following link.
Hi,
You can refer to the following thread post first:
It offered some solutions for slavefifo.