Announcements

Learn how to optimise USB-C for your designs at 18 May's USB-C PD Webinar.
Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

ArZa_1140216
Level 1
Level 1
First like given

Hello

Im using CyFwStorProg.exe to program my firmware to emmc. The process works fine on Win7 but on Windows 10 it seems that the process is completed successfully(see below log) but when rebooting the device keeps enumerating as cypress bootloader.

I have installed the win10 x64 drivers supplied with sdk1.3.4.

SUCCESS: Programmed Image "myimage.img" to Partition 0 in the Boot1 Location

SUCCESS: Reset device(with PMode[2:0] set to 0) to boot programmed firmware

FIN: Application Exiting.Press any key to continue . . .

Any thoughts??

1 Solution

Hey Arie,


I tried programming a eMMC using CyFwStorProg.exe in win10 x64 laptop and i was able to see that the device was enumerating as it was supposed to when booting from the eMMC.


Here's what i did to see this:

1.) From usage example of CyFwStorProg.exe, i firstly used, cyfwstorprog.exe -vid:04B4 -pid:00F3 -delpart

     A window will come up from file explorer asking to format the drive, please don't bother about it and let the .exe do its part.

2.) I then used the command, cyfwstorprog.exe -vid:04B4 -pid:00F3 -img:test1.img

     I didn't specify a boot partition and was able to successfully program the eMMC and got the debug messages like the ones that you mentioned.

3.) Changed the boot mode to eMMC->USB fallback mode by changing it from "Z11" to "000".

4.) Changed the connectots J21, J20, J25 and J26 from "SPI" to "SD CARD" and then "reset" the device.

5.) The device enumerated as expected.


Please do try the above method and share the findings with me.


Regards,

Yashwant

View solution in original post

0 Likes
3 Replies
YashwantK_46
Moderator
Moderator
Moderator
100 solutions authored 50 solutions authored 50 likes received

Hi,

Can you please take wireshark traces for both the instance and share them?


Also, can you please confirm that you are performing the exact same steps in both the versions of windows?

Also, please check for the PMODE lines when you are trying to boot from the emmc.

Regards,
Yashwant

0 Likes

Hi

Thanks for our response.

Unfortunately I cant get those traces right now..Any quick guide on ow to do so?

We've been doing the process for over 2 years with our devices on windows7 with no issues.

It seems o be something with win10.. Have you tried to program emmc with CyFwStorProg.exe on win10?

Regards,

Arie

0 Likes

Hey Arie,


I tried programming a eMMC using CyFwStorProg.exe in win10 x64 laptop and i was able to see that the device was enumerating as it was supposed to when booting from the eMMC.


Here's what i did to see this:

1.) From usage example of CyFwStorProg.exe, i firstly used, cyfwstorprog.exe -vid:04B4 -pid:00F3 -delpart

     A window will come up from file explorer asking to format the drive, please don't bother about it and let the .exe do its part.

2.) I then used the command, cyfwstorprog.exe -vid:04B4 -pid:00F3 -img:test1.img

     I didn't specify a boot partition and was able to successfully program the eMMC and got the debug messages like the ones that you mentioned.

3.) Changed the boot mode to eMMC->USB fallback mode by changing it from "Z11" to "000".

4.) Changed the connectots J21, J20, J25 and J26 from "SPI" to "SD CARD" and then "reset" the device.

5.) The device enumerated as expected.


Please do try the above method and share the findings with me.


Regards,

Yashwant

0 Likes