Two FX3 in JTAG chain + OpenOCD

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
lock attach
Attachments are accessible only for community members.
elwic_4042376
Level 1
Level 1
First like given

Hello,

I have two FX3 chips in a JTAG chain connected to OpenOCD. I use FT2232H module and OpenOCD 0.10.0. Cypress SDK 1.3.4.

...\OpenOCD-20181130\bin>openocd -f myftdi.cfg -f board.cfg

Open On-Chip Debugger 0.10.0 (2018-11-30) [https://github.com/sysprogs/openocd]

Licensed under GNU GPL v2

For bug reports, read

        http://openocd.org/doc/doxygen/bugs.html

trst_only separate trst_push_pull

jtag_ntrst_assert_width: 200

jtag_ntrst_delay: 200

RCLK - adaptive

adapter speed: 8000 kHz

fx3_1.cpu

Info : Listening on port 6666 for tcl connections

Info : Listening on port 4444 for telnet connections

Info : clock speed 8000 kHz

Info : JTAG tap: fx3_0.cpu tap/device found: 0x07926069 (mfg: 0x034 (Cypress), part: 0x7926, ver: 0x0)

Info : JTAG tap: fx3_1.cpu tap/device found: 0x07926069 (mfg: 0x034 (Cypress), part: 0x7926, ver: 0x0)

Info : Embedded ICE version 6

Info : fx3_0.cpu: hardware has 2 breakpoint/watchpoint units

Info : Embedded ICE version 6

Info : fx3_1.cpu: hardware has 2 breakpoint/watchpoint units

Info : Listening on port 3333 for gdb connections

Info : Listening on port 3334 for gdb connections

As you can see we have two ports 3333 and 3334 for gdb connection. I can debug first FX3 at 3333 port without any errors at all. But I can't access second FX3 at 3334.

OpenOCD hangs. I'm sure there is no signal integrity troubles at JTAG lines. Configuration files are attached.

Regards

0 Likes
1 Solution

Hi

Thank you for answer!

Previously I tried to run GDB OpenOCD Debugging (in Debug Configuration menu). For 3333 port it workes, but 3334 hangs.

Now I tried GDB Hardware Debugging with options:

GDB Command: arm-none-eabi-gdb

Use remote target - checked

JTAG Device: GNU ARM OpenOCD

Host name or IP address: localhost

Port number: 3333 (or 3334 for second device)

Force threread list update on suspend - checked

Both port debug works fine!

Regards

View solution in original post

0 Likes
2 Replies