Announcements

Learn how to optimise USB-C for your designs at 18 May's USB-C PD Webinar.
Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Anonymous
Not applicable

Hi 

   

Is there any way to raise the voltage level of TX +, TX- of USB3.0? 

I want to raise LEVEL using hardware and software. 

The current LEVEL is 0.25V and the LEVEL you want to raise is 0.3V. 

   

Thanks

1 Solution
Anonymous
Not applicable

CyU3PUsbSetTxSwing API sets the Tx amplitude used by FX3 on the USB 3.0 interface. Please use this API with caution. The device
has only been tested to work properly under the default swing setting of 0.9V (swing value set to 90). This API is
expected to be called before calling the CyU3PConnectState() API to enable USB connections. (swing TX Amplitude swing in 10 mV units. Should be less than 1.28V)

View solution in original post

0 Likes
1 Reply
Anonymous
Not applicable

CyU3PUsbSetTxSwing API sets the Tx amplitude used by FX3 on the USB 3.0 interface. Please use this API with caution. The device
has only been tested to work properly under the default swing setting of 0.9V (swing value set to 90). This API is
expected to be called before calling the CyU3PConnectState() API to enable USB connections. (swing TX Amplitude swing in 10 mV units. Should be less than 1.28V)

0 Likes