Schematic FX3S with EMMC

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
SePe_4029311
Level 1
Level 1
First like given

Hello.

1) The design guidelines recomends install on the SD cards and EMMC 22 Ohm resistors (page 27-28). For EMMC install the same on both sides of these resistors? Or they can not install?

2) Is it possible to supply the power supply unit (VIO3 (as schematic) directly from 1.8V, without switching 3.3->1.8 (page 28)?

3) It is possible to install a ferrite (MPZ2012S601A) with a size smaller, example 1A for example?

Best regards.

0 Likes
1 Solution
KandlaguntaR_36
Moderator
Moderator
Moderator
25 solutions authored 10 solutions authored 5 solutions authored

Hello,

1. Can you please re-state the question?

2. You can operate VIO3 at 1.8V. In general, UHS-1 type of SD cards needs 3.3 V at the starting and 1.8 V during data transfer. Since you are using eMMC, you can connect VIO3 to 1.8 V

3. Please use recommended Ferrite bead

View solution in original post

1 Reply
KandlaguntaR_36
Moderator
Moderator
Moderator
25 solutions authored 10 solutions authored 5 solutions authored

Hello,

1. Can you please re-state the question?

2. You can operate VIO3 at 1.8V. In general, UHS-1 type of SD cards needs 3.3 V at the starting and 1.8 V during data transfer. Since you are using eMMC, you can connect VIO3 to 1.8 V

3. Please use recommended Ferrite bead