Nov 06, 2018
06:18 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Nov 06, 2018
06:18 PM
Hello,
Is it possible to program SPI ROM for FX3 firmware without using Control Center?
If don't have any solution from cypress, how about any third party product?
Thanks
Solved! Go to Solution.
1 Solution
Nov 06, 2018
06:50 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Nov 06, 2018
06:50 PM
Hello,
The SPI slave that is used should match the following write commands for successful programming from the USB Control Center.
- Write Enable: 06h
- Write data (Page Program): 02h
- Sector Erase: D8h
In case the commands are different, the USB Control Center can be modified to suit the slave device that is used. The source of the control center can be found from the below path after the installation of FX3 SDK.
C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\application\c_sharp\controlcenter
Best regards,
Srinath S
1 Reply