- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I have the EZ-USB FX3 DVK. I am trying to debug it using the Cypress EZ USB Suite, and an Olimex ARM-USB-OCD-H.
I followed the instructions in the EZ-USB Suite Users Guide for using OpenOCD to debug. When ever I try to debug in the IDE I recieve the following error:
Open On-Chip Debugger 0.8.0 (2014-12-03-15:43)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.sourceforge.net/doc/doxygen/bugs.html
Warn : Adapter driver 'cy7c65215' did not declare which transports it allows; assuming legacy JTAG-only
Info : only one transport option; autoselect 'jtag'
adapter_nsrst_delay: 200
jtag_ntrst_delay: 200
adapter speed: 1000 kHz
trst_and_srst srst_pulls_trst srst_gates_jtag trst_push_pull srst_open_drain connect_deassert_srst
RCLK - adaptive
adapter speed: 1000 kHz
Error: CyJtagDevice Not found
in procedure 'init'
This is followed by:
Quit (expect signal SIGINT when the program is resumed)
Quit (expect signal SIGINT when the program is resumed)
Quit (expect signal SIGINT when the program is resumed)
Exception condition detected on fd 0
error detected on stdin
I've tried using a different config file, which I found on this site, and using the Olimex supplied openocd.exe, but nothing seems to work.
Can anyone help me out with this? I'm running out of ideas.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
OK, I mostly have it working. I switched over to using the Olimex openocd.exe. I'm not sure if that matters. I also specify a different config file, and olimex-arm-ocd-h.cfg in the config options:
And I had to alter the config file I found. There was a -variant switch in the file that wasn't valid. I'm not sure what the original author was trying to do, but I just removed the switch, and it seems to work.
Now I have one more issue.
I have "Start OpenOCD locally" checked, but it doesn't start it locally. I have to use the command line to start openocd.exe with the proper options, and leave it running in the command window. Then I can go back to the IDE, and debug.
Does anyone know how I can get the IDE to start openocd.exe for me when I begin a debug session?