Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anup
Level 1
Level 1
5 sign-ins First question asked Welcome!

We were testing of the Designing A GPIF™ II Master Interface concept using CYUSB3KIT-003 kit and try to send data from Slave to Master  and Master to Slave in line with the document AN87216. We observed that the transmission is happening in same PC having two USB 3.0 port.

But when we are connecting between two PC (One PC ->Host ,Second PC->Slave), the Slave USB device is not able to transfer data to Master USB and only master to slave data transfer is working.

 

How to transfer data from Slave to Host using CYUSB3KIT-003 kit between two PC?

 

0 Likes
1 Reply
Meghavi
Moderator
Moderator
Moderator
250 replies posted 100 solutions authored 10 likes received

Hi,

Can you please confirm if the default GPIF II state machine is used or not?

Also, please share the UART Debug prints of the both FX3 while the application is running.

Regards

0 Likes