MIPI CSI-2 V1.3 chip backwards compatibility with MIPI CSI-2 V1.01 Chip ( CYUSB3065-BZXC )

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
tp2693
Level 1
Level 1
First question asked Welcome!

Hi, 

We are using the DS90UB954TRGZTQ1 and DS90UB953 from TI for serializing and Deserializing MIPI data from a High-speed camera. To send the data to the computer we are using the CYUSB3065-BZXC from Cypress Semi because it has UVC drivers support. The CYUSB3065-BZXC supports only MIPI CSI-2 V1.01 whereas the DS90UB954 chip support MIPI-CSI 2 V1.3.

Is the MIPI CSI-2 V1.3 backward compatible with MIPI CSI-2 V1.01 ? Do I have to do any special configuration for this on the USB Super Speed Phy? Would I face any issues?

Tony 

0 Likes
1 Solution
JayakrishnaT_76
Moderator
Moderator
Moderator
First question asked 1000 replies posted 750 replies posted

Hello Tony,

Please refer to the following thread in which a similar thread was discussed before:

https://community.infineon.com/t5/USB-superspeed-peripherals/About-csi-2-version-in-CX3/m-p/283348

Best Regards,
Jayakrishna

View solution in original post

0 Likes
1 Reply
JayakrishnaT_76
Moderator
Moderator
Moderator
First question asked 1000 replies posted 750 replies posted

Hello Tony,

Please refer to the following thread in which a similar thread was discussed before:

https://community.infineon.com/t5/USB-superspeed-peripherals/About-csi-2-version-in-CX3/m-p/283348

Best Regards,
Jayakrishna
0 Likes