- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I use the FX3 contact to a spi chip,i use the spi with the DMA mode,the external chip need that the MOSI PIN of FX3 must be high level,but when i init the spi interface of the FX3,this pin is low level in the idel state.then i use the spi with the DMA mode to transfer and receive at the same time ,and when read data from the external chip ,i transfer oxff.but when i set to transfer and receive only one word,the CyU3PDmaChannelWaitForCompletion return is eeror(CY_U3P_ERROR_NOT_STARTED) ,
status = CyU3PDmaChannelSetupRecvBuffer (&glSpiRxHandle, &buf_p);
CyU3PDmaChannelSetupSendBuffer (&glSpiTxHandle,&s_buf);
CyU3PSpiSetBlockXfer (1, 1);
status = CyU3PDmaChannelWaitForCompletion (&glSpiRxHandle,
CY_FX_USB_SPI_TIMEOUT);
if (status == CY_U3P_ERROR_NOT_STARTED)
{
//CyU3PGpioSetValue(34,CyFalse);
}
status = CyU3PDmaChannelWaitForCompletion(&glSpiTxHandle,
CY_FX_USB_SPI_TIMEOUT);
if (status != CY_U3P_SUCCESS)
{
CyU3PGpioSetValue(37,CyFalse);
}
CyU3PSpiDisableBlockXfer (CyTrue, CyTrue);
can you tell me what is the problem?
thanks very much.