Using the GPIF designer, I configured the GPIF interface as master with internal clock.
It appears that the statemachine runs @ 200Mhz, and that the clock provided by the FX3 to the outside world is also 200Mhz.
I tried using CyU3PDeviceInit but that doesn't change the GPIF frequency
I tried changing the CY_U3P_GPIF_CONF_DDR_MODE field in the GPIF Configuration Register by manually changing the generated cyfxgpif2config.h file, but that doesn't help either..
In both cases the external clock remains 200.8Mhz ...
Q: Has anyone ideas how to change this to 100Mhz?
(since that is the maximum frequency the interface supports...)
I haven't used this but maybe another function to try is CyU3PPibInit(). See slavefifo example for some details about it.
Sodafarl
That seems to work, thanks!