- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I am developing project using CYUSB3KIT-003 and FMC interconnect board CYUSB3ACC-005. the USB FMC interconnect board(CYUSB3ACC-005) net name is CTL[12:0] |
Solved! Go to Solution.
- Labels:
-
ispn:38618:1:0
-
ispn:38621:1:0
-
l1:314:1:0
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
If you look into the "slaveFIFO2b_fpga_top.ucf" file in the AN65974 project you will find the mapping of each signal as follows:
"flaga" LOC = T7;
"flagb" LOC = M11;
"flagc" LOC = N11;
"flagd" LOC = N8;
"slcs" LOC = A7;
"pktend" LOC = M8
"sloe" LOC = P8;
"slrd" LOC = R7;
"slwr" LOC = N7;
"faddr[0]" LOC = N9;
"faddr[1]" LOC = M10;
Moreover I am attaching an image of interconnect board that will help you to map the signals.
Hope this will answer your question.
-Regards
Abhinav
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
You have to map the desired signals in "slaveFIFO2b_fpga_top.ucf" file. Please refer to the FPGA board Schematics and Interconnect Board Schematics to properly select the signals.
Thanks & Regards
Abhinav
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Thanks for your sincerely reply.
But I still do not get the desired answer.
I need the mapping relationship between ctl[12:0](in CYUSB3ACC-005) and below signals:
flaga,
flagb,
flagc,
flagd,
SLCS#,
PKTEND#,
SLRD#,
SLWR#,
SLOE#,
A[1:0], which are descripted in doc AN65974。
For example, in CYUSB3ACC-005, DQ0 pin is mapped with H4. In FPGA board Schematics, I can find the mapped signal of H4 in FMC JX is LA16_N. and then, LA16_N can be found mapped to AJ13 IN FPGA band10.
So I know DQ0 should be constrained to AJ13 in my .ucf file.
In doc EZ-USB FX3 Technical Reference Manual, spec No:001-76074 Rev. *E, about CTL[12:0] description is:
The GPIF II control signals (CTL[12:0]) can be configured as outputs to control the external peripheral device, or as inputs to read the status from an external peripheral device.
In doc AN 65974, EZ-USB FX3 used as slave FIFO connected to external FPGA. the interface between FX3 and FPGA is DQ[31:0], flaga, et al. I guess, there is a mapped relationship between and flaga and CTL[12:0].
But I didn't find the mapped relationship.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
If you look into the "slaveFIFO2b_fpga_top.ucf" file in the AN65974 project you will find the mapping of each signal as follows:
"flaga" LOC = T7;
"flagb" LOC = M11;
"flagc" LOC = N11;
"flagd" LOC = N8;
"slcs" LOC = A7;
"pktend" LOC = M8
"sloe" LOC = P8;
"slrd" LOC = R7;
"slwr" LOC = N7;
"faddr[0]" LOC = N9;
"faddr[1]" LOC = M10;
Moreover I am attaching an image of interconnect board that will help you to map the signals.
Hope this will answer your question.
-Regards
Abhinav