Hi:
I am use the FX3 as a usb controller to connect to a FPGA.I want to konw how to set DMA and endpoint that the pc host can transfer data to FPGA with the fast speed.Is the endpoint brust or streams?Can i set some dma channels to transfer data which is the whole?
Hi Wang,
Please refer to the FX3 application note AN87216.
http://www.cypress.com/documentation/application-notes/an87216-designing-gpif-ii-master-interface
Refer to the GPIF master project.
Thanks,
Krishna.