Hi,
By referencing SRAMMaster example, I've created a simple register read/write project.
Please note, I've swapped write initial state name (START) with read initial state (RD_START), since don't know how to start the read flow.
Like the example, I'm using AddressCounter as address source.
It's "working", but start address is tied to 0.
How can I set start address to any 32 bits value?
Solved! Go to Solution.
Hello Dong Chen,
--CyU3PGpifInitAddrCounter funtion is used in the firmware to configure the GPIF LD_ADDR_COUNT with the desired initial value, limit and counting mode.
This API should be called after GPIFLoad and before GPIFStart in the Firmware.
example : if you want to set start address to 10 and address limit to 255, you should set the initial value,limit and incerement value using following API.
void CyU3PGpifInitAddrCounter ( uint32_t initValue, uint32_t limit, CyBool_t reload, CyBool_t upCount, uint8_t increment )
uint32_t initValue = 0x0000000A
uint32_t limit = 0x000000FF
CyBool_t reload = CyTrue
CyBool_t upCount = CyTrue
uint8_t increment = 0x01
Regards,
Anil Srinivas.
Hello Dong Chen,
--CyU3PGpifInitAddrCounter funtion is used in the firmware to configure the GPIF LD_ADDR_COUNT with the desired initial value, limit and counting mode.
This API should be called after GPIFLoad and before GPIFStart in the Firmware.
example : if you want to set start address to 10 and address limit to 255, you should set the initial value,limit and incerement value using following API.
void CyU3PGpifInitAddrCounter ( uint32_t initValue, uint32_t limit, CyBool_t reload, CyBool_t upCount, uint8_t increment )
uint32_t initValue = 0x0000000A
uint32_t limit = 0x000000FF
CyBool_t reload = CyTrue
CyBool_t upCount = CyTrue
uint8_t increment = 0x01
Regards,
Anil Srinivas.