Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

USB superspeed peripherals Forum Discussions

QsLi_3517121
Level 1
Level 1

Hi,

Which API should I call?

Please give an example.

thank you!

0 Likes
1 Solution

Hi,

If any of the CTL[12:0] lines are used for GPIF interface they should not be configured as GPIOs. Similarly if some lines of CTL[12:0] are not used for GPIF they can be overridden to be GPIOs using the CyU3PDeviceGpioOverride call.

Regards,

Anil Srinivas.

View solution in original post

0 Likes
3 Replies
VlKh_2251656
Level 5
Level 5
10 likes given 5 likes given First like received

I think, not possible...

May be two pin?

0 Likes

But I could be wrong ...

0 Likes

Hi,

If any of the CTL[12:0] lines are used for GPIF interface they should not be configured as GPIOs. Similarly if some lines of CTL[12:0] are not used for GPIF they can be overridden to be GPIOs using the CyU3PDeviceGpioOverride call.

Regards,

Anil Srinivas.

0 Likes