- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I am facing an issue in 1.3.4 SDK at High speed, that the issue is if I build my code at 1.3.4 SDK there is a frame drop while opening the UVC control window. In 1.3.1 SDK version I am not facing this issue. As per my knowledge it is due the integration of bulk or ISO endpoint suspend logic in latest SDK version, so I need to disable that logic in SDK. So please guide me to achieve this.
Thanks and Regards,
Vignesh Kumar R.
Solved! Go to Solution.
- Labels:
-
USB Superspeed Peripherals
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
You can also refer to this thread USB endpoint EP0 low performance in SDK version 1_... - Cypress Developer Community with similar query.
The thread pointed mentions :
Instead of using CyU3PDmaChannelSendData() please test using CyU3PUsbSendEP0Data() itself - but along with this the following API needs to be used - CyU3PUsbSetEpSuspDisableMask() API (refer 5.36.7.52 of FX3 API guide) - which skips suspend of USB IN endpoints (as per the mask chosen).
But please note that by using CyU3PUsbSetEpSuspDisableMask(), there may be chances of data corruption when Bulk and EP0-IN transfers happen concurrently. Even when you used CyU3PDmaChannelSendData(), this possibility existed - which was communicated in the thread Solved: CYUSB3013 low control read performance with FX3 SD... - Cypress Developer Community.
Rashi
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
As mentioned in part IV of section 2.3 of FX3 trouble shooting guide, for concurrent BULK IN and EP0 IN transfers it is possible that the data sent on the control endpoint gets corrupted.
If the BULK IN transfers are not suspended, there is a possibility of control IN transfers getting corrupted.
To improve the performance of control IN transfers the workaround mentioned in following thread Solved: CYUSB3013 low control read performance with FX3 SD... - Cypress Developer Community can be followed.
Please let me know if this helps.
Rashi
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
You can also refer to this thread USB endpoint EP0 low performance in SDK version 1_... - Cypress Developer Community with similar query.
The thread pointed mentions :
Instead of using CyU3PDmaChannelSendData() please test using CyU3PUsbSendEP0Data() itself - but along with this the following API needs to be used - CyU3PUsbSetEpSuspDisableMask() API (refer 5.36.7.52 of FX3 API guide) - which skips suspend of USB IN endpoints (as per the mask chosen).
But please note that by using CyU3PUsbSetEpSuspDisableMask(), there may be chances of data corruption when Bulk and EP0-IN transfers happen concurrently. Even when you used CyU3PDmaChannelSendData(), this possibility existed - which was communicated in the thread Solved: CYUSB3013 low control read performance with FX3 SD... - Cypress Developer Community.
Rashi
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Rashi,
Thanks for your response, it worked.