Announcements

Learn how to optimise USB-C for your designs at 18 May's USB-C PD Webinar.
Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

dawa_2529456
Level 4
Level 4
5 sign-ins 5 solutions authored First solution authored

Dear Sir,

I add a compositive hid device in my CX3 UVC application according toAdding HID interface to AN75779 project attached demo Memo_CX3_UVC_HID_ButtonTrigger.zip.

I am glad to  see this HID device in device management tree(win10), but GPIO interrupt event cannot be triggered. so char "x" is not sent to PC.

The flowing code is form CX3_UVC_HID_ButtonTrigger.zip. the comments by mady is reserved and no modification. e.g. I use GPIO21 instead of GPIO17. and event group is glCx3Event, not glTimerEvent

void CyFxGpioIntrCb (

            uint8_t gpioId /* Indicates the pin that triggered the interrupt */

            )

{

        CyU3PReturnStatus_t apiRetStatus = CY_U3P_SUCCESS;

        cnt ++;

        apiRetStatus = CyU3PEventSet(&glCx3Event, INTERRUPT_TRIGGER,CYU3P_EVENT_OR);  //mady: This function is called when GPIO 17 is asserted or de-asserted

        //mady: We set the glTimerEvent flag that Key has been pressed

        if (apiRetStatus != CY_U3P_SUCCESS)

        {

        CyCx3UvcAppErrorHandler(apiRetStatus);

        }

}

CyFxGpioIntrCb() just set INTERRUPT_TRIGGER event, and then this event  will be dealed in CyCx3UvcAppThread_Entry() as well as other events. it is registered by CyU3PGpioInit() in CyCx3UvcAppInit().

CyCx3UvcAppInit(void)

{

// omitted

.....

.....

.....

.....

//

/* Init the GPIO module */

      gpioClock.fastClkDiv = 2;

      gpioClock.slowClkDiv = 0;

      gpioClock.simpleDiv = CY_U3P_GPIO_SIMPLE_DIV_BY_2;

      gpioClock.clkSrc = CY_U3P_SYS_CLK;

      gpioClock.halfDiv = 0;

      status = CyU3PGpioInit(&gpioClock, CyFxGpioIntrCb); //mady: specifying the callback function when the key (GPIO) is pressed

      if (status != 0)

      {

          /* Error Handling */

          CyU3PDebugPrint (4, "\n\rCyU3PGpioInit failed, error code = %x\n", status);

          CyU3PDebugPrint (4, "\n\rglIsGpioActive = %d\n", glIsGpioActive);

     //     esUVCAppErrorHandler(apiRetStatus);

      }

      status = CyU3PDeviceGpioOverride (21, CyTrue);  //mady : configuring GPIO 21 as Keyboard Key

      if (status != 0)

      {

          /* Error Handling */

          CyU3PDebugPrint (4, "CyU3PDeviceGpioOverride failed, error code = %d\n",

                  status);

          CyCx3UvcAppErrorHandler(status);

      }

     

     

       CyU3PGpioSimpleConfig_t gpioConfig;   

  

   gpioConfig.outValue = CyFalse;

    gpioConfig.driveLowEn = CyFalse;

    gpioConfig.driveHighEn = CyFalse;

    gpioConfig.inputEn = CyTrue;

    gpioConfig.intrMode = CY_U3P_GPIO_INTR_BOTH_EDGE;    //mady:COnfigure GPIO 21 for Interrupt. when it is asserted or de-asserted, it should send character 'x' to PC

    status = CyU3PGpioSetSimpleConfig(21, &gpioConfig);

    if (status != CY_U3P_SUCCESS)

    {

    /* Error handling */

       CyU3PDebugPrint (4, "CyU3PGpioSetSimpleConfig failed, error code = %d\n",status);

       CyCx3UvcAppErrorHandler(status);

    }

    else

    {

    CyU3PDebugPrint (1,"GPIO Cnfigured\n\r");

    }

}

So, How to make sure GPIO21 interrupt is working?  I cannot find error for  above gpio init procedure.

Does anyone give me some advice?

Thanks.

David

1 Solution

Please comment out MipiCsiInitializeGpio() APi as it internally calls GpioInit() function only.

View solution in original post

12 Replies
ManaskantD_51
Employee
Employee
Welcome! 25 solutions authored 10 solutions authored

The GPIO initialization code and the interrupt callback look ok. Can you perform hard reset in the interrupt callback by using CyU3PDeviceReset(CyFalse) API in the interrupt callback funciton? This is to make sure whether you are reaching till the interrupt callback or not.

0 Likes

Dear Sir,

I add   CyU3PDeviceReset(CyFalse)  in CyFxGpioIntrCb (), but it cannot solve this case. In fact , when  CyU3PGpioInit(&gpioClock, CyFxGpioIntrCb) is called in CyCx3UvcAppInit(), GpioInit failed, 0x43 is return. does this error make Gpiocb is not working?

David

void CyFxGpioIntrCb (

            uint8_t gpioId /* Indicates the pin that triggered the interrupt */

            )

{

        CyU3PReturnStatus_t apiRetStatus = CY_U3P_SUCCESS;

        cnt ++;

        CyU3PDeviceReset(CyFalse);

    //step 1: read GPIO44 value

    {

    CyBool_t gpioValue = CyFalse;

    CyU3PReturnStatus_t apiRetStatus = CY_U3P_SUCCESS;

    /* Get the status of the pin */

    apiRetStatus = CyU3PGpioGetValue (44, &gpioValue);

    if (apiRetStatus == CY_U3P_SUCCESS)

    {

    /* Check status of the pin */

    if (gpioValue == CyFalse) //GPIO44

    {

    /* Set CAM_INT1_INTERRUPT Event */

    apiRetStatus = CyU3PEventSet(&glCx3Event, CAM_INT1_INTERRUPT,

                        CYU3P_EVENT_OR);

    }

    }

            if (apiRetStatus != CY_U3P_SUCCESS)

            {

            CyCx3UvcAppErrorHandler(apiRetStatus);

            }

    /* Get the status of the pin */

    apiRetStatus = CyU3PGpioGetValue (45, &gpioValue);

    if (apiRetStatus == CY_U3P_SUCCESS)

    {

    /* Check status of the pin */

    if (gpioValue == CyFalse) //GPIO45

    {

    /* Set CAM_INT2_INTERRUPT Event */

    apiRetStatus = CyU3PEventSet(&glCx3Event, CAM_INT2_INTERRUPT,

                        CYU3P_EVENT_OR);

    }

    }

            if (apiRetStatus != CY_U3P_SUCCESS)

            {

            CyCx3UvcAppErrorHandler(apiRetStatus);

            }

    }

}

0 Likes

Initially, as you confirmed there is no error in GpioInit and Gpio configuration, I was suspecting the IntrCb or the Event Cb. The error code 0x43 indicates the Gpio module already started. Did you call the GpioInit() function before? You cannot call the GpioInit() twice.

0 Likes

Dear Sir,

I am sure GpioInit() is called just once, only in appinit(). I don't know why gpioinit failed with 0x43.

my gpiocb() is below: Gpio44 and Gpio 45 share one CyFxGpioIntrCb (), if Gpio44 interrupt occurs, CAM_INT1_INTERRUPT is set. and if Gpio45 interrupt occurs, CAM_INT2_INTERRUPT is set.

and these two event will be processed in CyCx3UvcAppThread_Entry () with other event flag, USB_supend and DMA timer out event.

void CyFxGpioIntrCb (

            uint8_t gpioId /* Indicates the pin that triggered the interrupt */

            )

{

        CyU3PReturnStatus_t apiRetStatus = CY_U3P_SUCCESS;

        cnt ++;

        CyU3PDeviceReset(CyFalse);

    //step 1: read GPIO44 value

    {

         CyBool_t gpioValue = CyFalse;

         CyU3PReturnStatus_t apiRetStatus = CY_U3P_SUCCESS;

    /     * Get the status of the pin */

         apiRetStatus = CyU3PGpioGetValue (44, &gpioValue);

         if (apiRetStatus == CY_U3P_SUCCESS)

         {

         /* Check status of the pin */

              if (gpioValue == CyFalse) //GPIO44

              {

                   /* Set CAM_INT1_INTERRUPT Event */

                        apiRetStatus = CyU3PEventSet(&glCx3Event, CAM_INT1_INTERRUPT,

                        CYU3P_EVENT_OR);

              }

         }

         if (apiRetStatus != CY_U3P_SUCCESS)

         {

            CyCx3UvcAppErrorHandler(apiRetStatus);

          }

         /* Get the status of the pin */

         apiRetStatus = CyU3PGpioGetValue (45, &gpioValue);

         if (apiRetStatus == CY_U3P_SUCCESS)

         {

              /* Check status of the pin */

              if (gpioValue == CyFalse) //GPIO45

              {

              /* Set CAM_INT2_INTERRUPT Event */

                        apiRetStatus = CyU3PEventSet(&glCx3Event, CAM_INT2_INTERRUPT,

                        CYU3P_EVENT_OR);

              }

         }

         if (apiRetStatus != CY_U3P_SUCCESS)

          {

                CyCx3UvcAppErrorHandler(apiRetStatus);

           }

    }

}

my gpioinit procedure is : gpio44 is overide,and gpio45 is IOmatrix conifg,it is called at the end of appinit();

void Gpioinit()

{

  /* Init the GPIO module */

      gpioClock.fastClkDiv = 2;

      gpioClock.slowClkDiv = 0;

      gpioClock.simpleDiv = CY_U3P_GPIO_SIMPLE_DIV_BY_2;

      gpioClock.clkSrc = CY_U3P_SYS_CLK;

      gpioClock.halfDiv = 0;

      status = CyU3PGpioInit(&gpioClock, CyFxGpioIntrCb); //mady: specifying the callback function when the key (GPIO) is pressed

      if (status != 0)

      {

          /* Error Handling */

          CyU3PDebugPrint (4, "\n\rCyU3PGpioInit failed, error code = %x\n", status);

     //     esUVCAppErrorHandler(apiRetStatus);

      }

      CyU3PGpioSimpleConfig_t gpioConfig;

      status = CyU3PDeviceGpioOverride (44, CyTrue);  //mady : configuring GPIO 44 as CAM1_INT

      if (status != 0)

      {

          /* Error Handling */

          CyU3PDebugPrint (4, "CyU3PDeviceGpioOverride failed, error code = %d\n",

                  status);

          CyCx3UvcAppErrorHandler(status);

      }

      gpioConfig.outValue = CyTrue;

      gpioConfig.driveLowEn = CyFalse;

      gpioConfig.driveHighEn = CyFalse;

      gpioConfig.inputEn = CyTrue;

      gpioConfig.intrMode = CY_U3P_GPIO_INTR_NEG_EDGE; //CY_U3P_GPIO_INTR_LOW_LEVEL;  //mady:COnfigure GPIO 45 for Interrupt. when it is asserted or de-asserted, it should send character 'x' to PC

      status = CyU3PGpioSetSimpleConfig(44, &gpioConfig);

      if (status != CY_U3P_SUCCESS)

      {

      /* Error handling */

         CyU3PDebugPrint (4, "CyU3PGpioSetSimpleConfig44 failed, error code = %d\n",status);

         CyCx3UvcAppErrorHandler(status);

      }

      else

      {

      CyU3PDebugPrint (1,"GPIO44 Cnfigured\n\r");

      }

    gpioConfig.outValue = CyTrue;

    gpioConfig.driveLowEn = CyFalse;

    gpioConfig.driveHighEn = CyFalse;

    gpioConfig.inputEn = CyTrue;

    gpioConfig.intrMode = CY_U3P_GPIO_INTR_NEG_EDGE;   //mady:COnfigure GPIO 45 for Interrupt. when it is asserted or de-asserted, it should send character 'x' to PC

    status = CyU3PGpioSetSimpleConfig(45, &gpioConfig);

    if (status != CY_U3P_SUCCESS)

    {

    /* Error handling */

       CyU3PDebugPrint (4, "CyU3PGpioSetSimpleConfig45 failed, error code = %d\n",status);

       CyCx3UvcAppErrorHandler(status);

    }

    else

    {

    CyU3PDebugPrint (1,"GPIO45 Cnfigured\n\r");

    }

}

GpioEevenCb is in AppThreadEntry()

CyCx3UvcAppThread_Entry (

        uint32_t input)

{

    uint16_t wakeReason;

    uint32_t eventFlag;

    CyU3PReturnStatus_t status;

#ifdef PRINT_FRAME_INFO

    uint32_t fps;

    CyU3PMipicsiErrorCounts_t errCnts;

#endif

    /* Initialize the Debug Module */

    CyCx3UvcAppDebugInit();

    /* Initialize the UVC Application */

    CyCx3UvcAppInit();

    for (;;)

    {

        eventFlag = 0;

        //

        //  ........

         // ..........

    status = CyU3PEventGet (&glCx3Event,CX3_USB_SUSP_EVENT_FLAG|CAM_INT1_INTERRUPT|CAM_INT2_INTERRUPT|CX3_DMA_RESET_EVENT, CYU3P_EVENT_OR_CLEAR, &eventFlag, CYU3P_WAIT_FOREVER);

(status == CY_U3P_SUCCESS)

        {

            if( eventFlag & CAM_INT1_INTERRUPT)   //mady: check if key has been pressed

       {

          //.............................................................................

         }

     /./......

I review code line by line with CX3 demo code. it seems no different between them, but GPIO event cannot be received. and gpioinit() is called only once.

David

0 Likes

Please share your CX3 code project files.

0 Likes

Dear Sir,

My code cannot work in CX3 RDK normally because of my hardware is not comptible with CX3 RDK.

I simplify MyGpioInit() init with no interrupt enable and no gpio call back. just config gpiio44 ,gpio45(Gpio45 is configured in main() ) as input pin, and then call it in CyCx3UvcAppInit().  the first code is calling MyGpioInit().

the console show:

GPIO44 Cnfigured

GPIO45 Cnfigured

AppInit:GPIOInit Err = 0x43

and then Halt..

I test MyGpioInit() in CX3 demo code , it still occur same error, can you  paste MyGpioInit() in your CX3 code, and test why gpioinit() return 0x43?

void

CyCx3UvcAppInit (

        void)

{

    CyU3PEpConfig_t endPointConfig;

    CyU3PDmaMultiChannelConfig_t dmaCfg;

    CyU3PReturnStatus_t status = CY_U3P_SUCCESS;

#ifdef CX3_DEBUG_ENABLED

    CyU3PMipicsiCfg_t readCfg;

    CyU3PMipicsiErrorCounts_t errCnts;

#endif

   MyGpioInit();

    /* Initialize the I2C interface for Mipi Block Usage and Camera. */

    status = CyU3PMipicsiInitializeI2c (CY_U3P_MIPICSI_I2C_400KHZ);

    if(status != CY_U3P_SUCCESS)

    {

        CyU3PDebugPrint (4, "\n\rAppInit:I2CInit Err = 0x%x.",status);

        CyCx3UvcAppErrorHandler(status);

    }

.................................................

................................................

................................................

void MyGpioInit()

{

  CyU3PReturnStatus_t status = CY_U3P_SUCCESS;

/* Init the GPIO module */

  CyU3PGpioClock_t gpioClock;

  gpioClock.fastClkDiv = 2;

  gpioClock.slowClkDiv = 0;

  gpioClock.simpleDiv = CY_U3P_GPIO_SIMPLE_DIV_BY_2;

  gpioClock.clkSrc = CY_U3P_SYS_CLK;

  gpioClock.halfDiv = 0;

  status = CyU3PGpioInit(&gpioClock, NULL); //mady: specifying the callback function when the key (GPIO) is pressed

  if (status != 0)

  {

      /* Error Handling */

      CyU3PDebugPrint (4, "\n\rCyU3PGpioInit failed, error code = %x\n", status);

//     esUVCAppErrorHandler(apiRetStatus);

  }

  CyU3PGpioSimpleConfig_t gpioConfig;

  status = CyU3PDeviceGpioOverride (44, CyTrue);  //mady : configuring GPIO 44 as CAM1_INT

  if (status != 0)

  {

      /* Error Handling */

      CyU3PDebugPrint (4, "CyU3PDeviceGpioOverride failed, error code = %d\n",

              status);

      CyCx3UvcAppErrorHandler(status);

  }

gpioConfig.outValue = CyTrue;

  gpioConfig.driveLowEn = CyFalse;

  gpioConfig.driveHighEn = CyFalse;

  gpioConfig.inputEn = CyTrue;

  gpioConfig.intrMode = CY_U3P_GPIO_NO_INTR;//CY_U3P_GPIO_INTR_NEG_EDGE; //CY_U3P_GPIO_INTR_LOW_LEVEL;  //mady:COnfigure GPIO 45 for Interrupt. when it is asserted or de-asserted, it should send character 'x' to PC

  status = CyU3PGpioSetSimpleConfig(44, &gpioConfig);

  if (status != CY_U3P_SUCCESS)

  {

  /* Error handling */

     CyU3PDebugPrint (4, "CyU3PGpioSetSimpleConfig44 failed, error code = %d\n",status);

     CyCx3UvcAppErrorHandler(status);

  }

  else

  {

  CyU3PDebugPrint (1,"GPIO44 Cnfigured\n\r");

  }

gpioConfig.outValue = CyTrue;

gpioConfig.driveLowEn = CyFalse;

gpioConfig.driveHighEn = CyFalse;

gpioConfig.inputEn = CyTrue;

gpioConfig.intrMode = CY_U3P_GPIO_NO_INTR;//CY_U3P_GPIO_INTR_NEG_EDGE;//CY_U3P_GPIO_NO_INTR;//CY_U3P_GPIO_INTR_NEG_EDGE;    //mady:COnfigure GPIO 45 for Interrupt. when it is asserted or de-asserted, it should send character 'x' to PC

status = CyU3PGpioSetSimpleConfig(45, &gpioConfig);

if (status != CY_U3P_SUCCESS)

{

/* Error handling */

   CyU3PDebugPrint (4, "CyU3PGpioSetSimpleConfig45 failed, error code = %d\n",status);

   CyCx3UvcAppErrorHandler(status);

}

else

{

CyU3PDebugPrint (1,"GPIO45 Cnfigured\n\r");

}

}

Please copy MyGpioInit() into your CX code ,test whether Gpioinit  return 0x43.

Thanks!

David

0 Likes

Dear Sir,

GPIO45 is matrix configured in main(),GPIO44 must be override and cannot be matrix config.

/*

* Main function

*/

int

main (

        void)

{

    CyU3PIoMatrixConfig_t io_cfg;

    CyU3PReturnStatus_t status = CY_U3P_SUCCESS;

    /* Initialize the device */

    status = CyU3PDeviceInit (NULL);

    if (status != CY_U3P_SUCCESS)

    {

        goto handle_fatal_error;

    }

    /* Initialize the caches. Enable instruction cache and keep data cache disabled.

     * The data cache is useful only when there is a large amount of CPU based memory

     * accesses. When used in simple cases, it can decrease performance due to large

     * number of cache flushes and cleans and also it adds to the complexity of the

     * code. */

    status = CyU3PDeviceCacheControl (CyTrue, CyFalse, CyFalse);

    if (status != CY_U3P_SUCCESS)

    {

        goto handle_fatal_error;

    }

    /* Configure the IO matrix for the device.*/

    io_cfg.isDQ32Bit = CyFalse;

    io_cfg.useUart   = CyTrue;

    io_cfg.useI2C    = CyTrue;

    io_cfg.useI2S    = CyFalse;

    io_cfg.useSpi    = CyFalse;

    io_cfg.lppMode   = CY_U3P_IO_MATRIX_LPP_DEFAULT;

    /* No GPIOs are enabled. */

    io_cfg.gpioSimpleEn[0]  = 0;

    io_cfg.gpioSimpleEn[1]  = 0x00002000;

    io_cfg.gpioComplexEn[0] = 0;

    io_cfg.gpioComplexEn[1] = 0;

    status = CyU3PDeviceConfigureIOMatrix (&io_cfg);

    if (status != CY_U3P_SUCCESS)

    {

        goto handle_fatal_error;

    }

    /* This is a non returnable call for initializing the RTOS kernel */

    CyU3PKernelEntry ();

    /* Dummy return to make the compiler happy */

    return 0;

handle_fatal_error:

    /* Cannot recover from this error. */

    while (1);

}

0 Likes

Dear Sir,

MyGpioInit() is called in the beginning of CyCx3UvcAppInit(), it is OK, no error return, but when CyU3PMipicsiInitializeI2c () is called, its return is 0x43,  so I think CyU3PGpioInit() is called by CyU3PMipicsiInitializeI2c ();  so the console show:

GPIO44 Cnfigured

GPIO45 Cnfigured

AppInit:GPIOInit Err = 0x43

then go to error handler, while(1).

Can you test MyGpioInit() in CX3 demo code? can you make sure CyU3PMipicsiInitializeI2c () doesn't call CyU3PGpioInit() internally?

David

CyCx3UvcAppInit (

        void)

{

    CyU3PEpConfig_t endPointConfig;

    CyU3PDmaMultiChannelConfig_t dmaCfg;

    CyU3PReturnStatus_t status = CY_U3P_SUCCESS;

#ifdef CX3_DEBUG_ENABLED

    CyU3PMipicsiCfg_t readCfg;

    CyU3PMipicsiErrorCounts_t errCnts;

#endif

   MyGpioInit();

    /* Initialize the I2C interface for Mipi Block Usage and Camera. */

    status = CyU3PMipicsiInitializeI2c (CY_U3P_MIPICSI_I2C_400KHZ);

    if(status != CY_U3P_SUCCESS)

    {

        CyU3PDebugPrint (4, "\n\rAppInit:I2CInit Err = 0x%x.",status);

        CyCx3UvcAppErrorHandler(status);

    }

0 Likes

Dear Sir,

From console shows:  CyU3PMipicsiInitializeGPIO() call CyU3PGpioInit() internally. the error AppInit:GPIOInit Err = 0x43 is printed followed by calling CyU3PMipicsiInitializeGPIO().

GPIO44 Cnfigured

GPIO45 Cnfigured

AppInit:GPIOInit Err = 0x43

void

CyCx3UvcAppInit (

        void)

{

    CyU3PEpConfig_t endPointConfig;

    CyU3PDmaMultiChannelConfig_t dmaCfg;

    CyU3PReturnStatus_t status = CY_U3P_SUCCESS;

#ifdef CX3_DEBUG_ENABLED

    CyU3PMipicsiCfg_t readCfg;

    CyU3PMipicsiErrorCounts_t errCnts;

#endif

    MyGpioInit();

    /* Initialize the I2C interface for Mipi Block Usage and Camera. */

    status = CyU3PMipicsiInitializeI2c (CY_U3P_MIPICSI_I2C_400KHZ);

    if(status != CY_U3P_SUCCESS)

    {

        CyU3PDebugPrint (4, "\n\rAppInit:I2CInit Err = 0x%x.",status);

        CyCx3UvcAppErrorHandler(status);

    }

    /* Initialize GPIO module. */

    //MyGpioInit();

    status = CyU3PMipicsiInitializeGPIO ();

    if( status != CY_U3P_SUCCESS)

    {

        CyU3PDebugPrint (4, "\n\rAppInit:GPIOInit Err = 0x%x",status);

        CyCx3UvcAppErrorHandler(status);

    }

    /* Initialize the PIB block */

    status = CyU3PMipicsiInitializePIB ();

    if (status != CY_U3P_SUCCESS)

    {

        CyU3PDebugPrint (4, "\n\rAppInit:PIBInit Err = 0x%x",status);

        CyCx3UvcAppErrorHandler(status);

    }

0 Likes

Please comment out MipiCsiInitializeGpio() APi as it internally calls GpioInit() function only.

Dear Sir,

I see the comments about MipiCsiInitializeGpio(), it said GpioInit() is called internally.

But if I uncomment MipiCsiInitializeGpio() in Appinit(), an ERROR  occur:  AppInit:MipicsiInit Err =0x42

The app is not working normally.

CyU3PUsbGetSpeed() return CY_U3P_SUPER_SPEED!

bRType = 0x81, bRequest = 0x0, wValue = 0x0, wIndex = 0x0, wLength= 0x2

bRType = 0x81, bRequest = 0x0, wValue = 0x0, wIndex = 0x2, wLength= 0x2

bRType = 0x1, bRequest = 0x3, wValue = 0x0, wIndex = 0x100, wLength= 0x0

StpCB:In SET_FTR 0::1

bRType = 0x21, bRequest = 0xA, wValue = 0x0, wIndex = 0x2, wLength= 0x0

bRType = 0x81, bRequest = 0x6, wValue = 0x2200, wIndex = 0x2, wLength= 0x7F0 6

AppInit:GpifSMStart passed

AppInit:MipicsiInit Err = 0x42

bRType = 0x2, bRequest = 0x1, wValue = 0x0, wIndex = 0x85, wLength= 0x0

0 Likes

Dear Sir,

I solve this issue.

I uncomment MipiCsiInitializeGpio() and call MyGpioInit().

My code can receive GPIO EVENT now.

Thanks!

0 Likes