Announcements

Learn how to optimise USB-C for your designs at 18 May's USB-C PD Webinar.
Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

user_609701
Level 1
Level 1

I want to use GPIF-II to interface to a device with a 4-bit parallel bus and a 5-pin JTAG. The device needs to be configured via JTAG first. Is it possible to add a JTAG state-machine into GPIF-II ? Once configured via JTAG I then want to capture date from the 4-bit parallel bus

1 Solution

Hi,

You can't import Verilog SM directly into the GPIF II, you have to design your own SM using GPIF II designer tool.

You can make use of maximum 256 states in one GPIF project.

For more info on GPIF designer tool see C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\doc\GPIFII_Designer\ gpif2_designer_userguide.pdf

Thanks & Regards

Abhinav

View solution in original post

0 Likes
3 Replies
abhinavg_21
Moderator
Moderator
Moderator
50 likes received 25 likes received 10 likes received

Hi,

Yes you can implement JTAG in GPIF state machine but we don't have any example for it.

You can implement both(JTAG & 4 bit parallel data fetching) state machines in same project but with different starting state. You can choose the start state while loading the GPIF SM using CyFx3BootGpifLoad().

Please note one thing that GPIF II can have minimum of 8 bit parallel bus width.

Thanks & Regards
Abhinav

Thanks. Very helpful. Is there a way to import an existing VHDL/VERILOG JTAG statemachine (which I have) in to GPIF II or do I need to use the Cypress UX ?             What is the capacity of GPIF II ?

0 Likes

Hi,

You can't import Verilog SM directly into the GPIF II, you have to design your own SM using GPIF II designer tool.

You can make use of maximum 256 states in one GPIF project.

For more info on GPIF designer tool see C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\doc\GPIFII_Designer\ gpif2_designer_userguide.pdf

Thanks & Regards

Abhinav

0 Likes