Hi,
在我们的板子上通过CyUSB3035来访问MicroSD插槽(只有一个),VIO2提供3.3V电压。
其中,MicroSD的引脚如下图:
我将FX3SMassStorage例程修改后,下载到CyUSB3035中运行,调试信息返回“StorageQueryDev (0) failed with code 0x68”。
FX3SMassStorage例程主要修改如下:
1、#define LOG_ENABLE
2、int main(void)
/* Configure the IO matrix for the device.
* S0 port is enabled in 8 bit mode.
* S1 port is enabled in 4 bit mode.
* UART is enabled on remaining pins of the S1 port.
*/
io_cfg.isDQ32Bit = CyFalse;
io_cfg.s0Mode = CY_U3P_SPORT_4BIT;
#ifdef LOG_ENABLE
/* If the UART is used for logging, we can only configure the S1 port as 4 bits wide. */
io_cfg.s1Mode = CY_U3P_SPORT_INACTIVE;
io_cfg.lppMode = CY_U3P_IO_MATRIX_LPP_UART_ONLY;
io_cfg.useUart = CyTrue;
#else
io_cfg.s1Mode = CY_U3P_SPORT_8BIT;
io_cfg.lppMode = CY_U3P_IO_MATRIX_LPP_NONE;
io_cfg.useUart = CyFalse;
#endif
io_cfg.gpioSimpleEn[0] = 0;
io_cfg.gpioSimpleEn[1] = 0;//x02102800; /* IOs 43, 45, 52 and 57 are chosen as GPIO. */
io_cfg.gpioComplexEn[0] = 0;
io_cfg.gpioComplexEn[1] = 0;
io_cfg.useI2C = CyFalse;
io_cfg.useI2S = CyFalse;
io_cfg.useSpi = CyFalse;
status = CyU3PDeviceConfigureIOMatrix (&io_cfg);
if (status != CY_U3P_SUCCESS)
{
goto handle_fatal_error;
}
3、void CyFxMscApplnSibInit (void)
intfParams.resetGpio = 0xFF; /* No GPIO control on SD/MMC power. */
intfParams.rstActHigh = CyTrue; /* Don't care as no GPIO is selected. */
intfParams.cardDetType = CY_U3P_SIB_DETECT_DAT_3; /* Card detect based on SD_DAT[3]. */
intfParams.voltageSwGpio = 0xFF; /* Use GPIO_45 for voltage switch on S0 port. */
intfParams.lvGpioState = CyFalse; /* Driving GPIO low selects 1.8 V on SxVDDQ. */
intfParams.writeProtEnable = CyFalse; /* Write protect handling enabled. */
intfParams.lowVoltage = CyFalse; /* Low voltage operation enabled. */
intfParams.useDdr = CyTrue; /* DDR clocking enabled. */
intfParams.maxFreq = CY_U3P_SIB_FREQ_104MHZ; /* No S port clock limitation. */
intfParams.cardInitDelay = 0; /* No SD/MMC initialization delay required. */
status = CyU3PSibSetIntfParams (0, &intfParams);
if (status != CY_U3P_SUCCESS)
{
AppDebugPrint (4, "Set S0 SIB interface parameters failed, code=0x%x\r\n", status);
CyFxAppErrorHandler (status);
}
status = CyU3PSibStart ();
if (status != CY_U3P_SUCCESS)
{
AppDebugPrint (4, "SIB start failed, code=0x%x\r\n", status);
CyFxAppErrorHandler (status);
}
可以识别到大容量存储设备,但是无法连接到SD卡。
已解决! 转到解答。
由于只使用一个S0 port,所以VIO2供电3.3V,VIO3没有供电,VIO4供电1.8V。
VIO2供电必须是3.3V,启动时必须要3.3V,如果支持低电压,则动态修改为1.8V;VIO4供电始终是1.8V,我在例程中使用串口打印调试信息,后期会使用SPI。
现在我的板子和串口都是分别直接连接到PC的USB 3.0接口,使用FX3SFileSystem例程可以正确读写SD卡。之前我的板子和串口都是通过一个USB Hub连接到PC的,而且Hub没有外接电源,我想这是之前出现问题的主要原因。
希望能给其他遇到类似问题的人提供帮助。