Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

USB superspeed peripherals Forum Discussions

gean_3054931
Level 5
Level 5
10 likes given 5 likes given First like received

hello,

   As discussed in the previous post(FX3 SPI COMPATIBILITY ),those are supports 1.8v and 3.0v.

Is any spi flash that supports 3.3V Poer supply?

regards,

geetha.

0 Likes
1 Solution

Hi,

W25X40CLSNIG spi flash support 3.3v power supply and compatible to Fx3.

Regards,

Anil Srinivas.

View solution in original post

0 Likes
5 Replies
alamandaa_16
Moderator
Moderator
Moderator
10 likes received First like received

Hi Geetha,

MX25R8035F spi flash support 3.3v power supply.

Regards,

Anil Srinivas.

  Hello Anil,

thanks for the replay.

it should satisfy the commands and compatibility with fx3s(cyusb3035)?

how can i check commands compatibility with the spi flash?

reagrds,

geetha.

0 Likes

Hi,

Please go through the below link which speaks about the SPI Flash compatibility and the command set:

Selection of SPI Flash Compatible with FX3/CX3/FX3S/FX2G2/SD3/SD2 and the Recommended Cypress SPI Fl...

Regards,

Anil Srinivas.

Hello anil srinivas,

MX25R8035F spi flash (3.3v power supply).This device is not available.

can you tell me other spi part number that are compatible to fx3?

currently which spi part number is used in FX3 dvk?

regards,

geetha.

0 Likes

Hi,

W25X40CLSNIG spi flash support 3.3v power supply and compatible to Fx3.

Regards,

Anil Srinivas.

0 Likes