who can tell me , the fx3 how to detected the speed,
CyU3PUsbGetSpeed
oh,you may not understand my question.
My fx3 board linked to PC,but PC treat it as a USB2.0 device,so the speed is slow.
My PC has a USB3.0 interface.
Are you using a custom board or the DVK?
What firmware have you downloaded onto FX3?
Regards,
Anand
Hi,
I have encountered the same probelm.
My PC enumerates other USB 3.0 device as a SupterSpeed but it enumerate the FX3 DVK as a HighSpeed device.
I tried with UVC FW and default WestBridge FW.
UVC FW -> view with USB device viewer:
Current Config Value: 0x01 -> Device Bus Speed: High
default WestBridge FW -> Cypress Control Center:
<DEVICE>
FriendlyName="Cypress USB BootLoader"
Manufacturer="Cypress"
Product="WestBridge "
SerialNumber="0000000004BE"
Configurations="1"
MaxPacketSize="64"
VendorID="04 B4"
ProductID="00 F3"
Class="00h"
SubClass="00h"
Protocol="00h"
BcdDevice="01 00"
BcdUSB="02 00"
That is strange. With the DVK you shouldn't be seeing this. Please create a tech support case (MyAccount -> MyCases) so that one of our engineers can take a look at this.
Regards,
Anand
Hello
I using a custom board.
I have the same probelm.
using the Control Center, then the window is showed
<DEVICE>
FriendlyName="Cypress USB BootLoader"
Manufacturer="Cypress"
Product="WestBridge "
SerialNumber="0000000004BE"
Configurations="1"
MaxPacketSize="64"
VendorID="04 B4"
ProductID="00 F3"
Class="00h"
SubClass="00h"
Protocol="00h"
BcdDevice="01 00"
BcdUSB="02 00"
the result is is different from Control Center User's Guide .
And I can not use the I2C boot option
The board's EEPROM is 24LC512 and the download fw is C:\Cypress\Cypress SuperSpeed USBSuite\bin\CyBootProgrammer.img
thanks.
Supplement
I setting the PMOD[2:0] is F1F ( I2C, on failure, USB boot is enable)
hi! jogn_li,gary,eknngx,have any of you solved the problem?can you tell me?
i have confuse on the problem too
First you must confirm that your PC has the interface of USB3.0 .
If not,you can buy a PCIE Adpter Card.
my fault ,,PCI Adapter Card
i have also only usb 2
BcdUSB="02 00"
with win732 and a renesas usb3.0 pcie 2 port card, (NEC720200F Chip) Driver 2.1.28.0 FW. 3028
is the card working with usb3.0 and the cy3014 ?
I COLLECTED WITH THE SAME PROBLEM.
IT IS THE PROBLEM OF THE COMPUTER, MOST PORT USB3 IS NOT VERY GOOD.
I WILL NOT CASE ANY EXAMPLES TO NOT HURT THE REPUTATION OF MANUFACTURER MAKES.