Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
mimic_2725621
Level 1
Level 1

Hello,

I downloaded drivers for FX3 from

Drivers for EZ-USB® FX1™ , FX2LP™ , and FX3™ - KBA94413

Also i did try to install FX3SDKSetup_1.3.4.exe to find correct driver.

In both cases i have problems with installation driver for winXP 32 bit.

In ...Cypress\EZ-USB FX3 SDK\1.3\driver\bin\wxp\x86 there are set of files including WdfCoInstaller01009.dll. BUT...cyusb3.inf inside required WdfCoInstaller01011.dll

So in result installation false. Even i would change file name WdfCoInstaller01011.dll on 009, result of installation the same - error.

Could someone tell:

1. Is there drivers for FX3 and Windows XP which is installed and WORKED correctly?

2. Why drivers in archive require win usb 1.11 but have version 1.9 in installation folder?

WBR,

0 Likes
1 Solution

Hello,

We are looking into the issue on the WDF co-installer version miss-match in the inf file. We will update this soon.

For wxp driver installation please download and install USBSerialSDKSetup.exe from this link

and use the driver present in " C:\Program Files (x86)\Cypress\USB-Serial SDK\Cypress USB-Serial Driver\DriverBinary\Vendor_Driver\bin\wxp\<architecture> "

Best Regards,

Yatheesh

View solution in original post

0 Likes
7 Replies
YatheeshD_36
Moderator
Moderator
Moderator
750 replies posted 500 replies posted 250 solutions authored

Hello Mikchel,

We will look into the WDF co-installer version for wxp in the driver package.

Please replace "WdfCoinstaller01009.dll" in Cypress\EZ-USB FX3 SDK\1.3\driver\bin\wxp\x86  with WdfCoinstaller01011.dll from Cypress\EZ-USB FX3 SDK\1.3\driver\bin\win7\x86 and try installing the driver.

Best Regards,

Yatheesh

0 Likes

Hi. This was what i did first. Not to disturb forum, but solve problem by

your self.

Driver in result completed installation, but with error. So FX3 device is

not accesible.

That is why i asked for support.

YatheeshK_36 <community-manager@cypress.com> 21 июня 2019 г. 7:09:57 ПП

написал:

Cypress Developer Community

>

FX3 driver for WinXP 32 bit

reply from YatheeshK_36 in USB Superspeed Peripherals - View the full

discussion

Hello Mikchel,

We will look into the WDF co-installer version for wxp in the driver package.

Please replace "WdfCoinstaller01009.dll" in Cypress\EZ-USB FX3

SDK\1.3\driver\bin\wxp\x86 with WdfCoinstaller01011.dll from

Cypress\EZ-USB FX3 SDK\1.3\driver\bin\win7\x86 and try installing the driver.

Best Regards,

Yatheesh

Reply to this message by replying to this email, or go to the message on

Cypress Developer Community

Start a new discussion in USB Superspeed Peripherals by email or at Cypress

Developer Community

Following FX3 driver for WinXP 32 bit in these streams: Inbox

This email was sent by Cypress Developer Community because you are a

registered user.

You may unsubscribe instantly from Cypress Developer Community, or adjust

email frequency in your email preferences

0 Likes

Installation of driver complete with message that "Unable to init driver fot that device (code 37)".

In windows events there is a record:from Wdf01011:

Тип события:    Предупреждение

Источник события:    Wdf01000

Категория события:    Отсутствует

Код события:    1

Дата:        24.06.2019

Время:        10:53:20

Пользователь:        Н/Д

Компьютер:    RUMJANTSEV-DEV

Описание:

Не найдено описание для события с кодом ( 1 ) в источнике ( Wdf01000 ). Возможно, на локальном компьютере нет нужных данных в реестре или файлов DLL сообщений для отображения сообщений удаленного компьютера. Попробуйте использовать ключ /AUXSOURCE= для получения этого описания, - дополнительные сведения об этом содержатся в справке. В записи события содержится следующая информация: ; Driver Version: 1.11 Kmdf Lib. Version: 1.9.

Данные:

0000: 00 00 10 00 02 00 62 00   ......b.

0008: 00 00 00 00 01 00 07 80   .......€

0010: 00 00 00 00 24 00 00 c0   ....$..À

0018: 00 00 00 00 00 00 00 00   ........

0020: 00 00 00 00 00 00 00 00   ........

0028: 01 00 00 00 0b 00 00 00   ........

0030: 01 00 00 00 09 00 00 00   ........

Sorry...it is in Russian but i think generally it is ok to understand that driver could not run correctly.

I do not understand the following line:

Driver Version: 1.11 Kmdf Lib. Version: 1.9.

Does it mean that i have older usb library than driver required?

0 Likes

Hello,

We are looking into the issue on the WDF co-installer version miss-match in the inf file. We will update this soon.

For wxp driver installation please download and install USBSerialSDKSetup.exe from this link

and use the driver present in " C:\Program Files (x86)\Cypress\USB-Serial SDK\Cypress USB-Serial Driver\DriverBinary\Vendor_Driver\bin\wxp\<architecture> "

Best Regards,

Yatheesh

0 Likes

Thank you for link,,,,,but after installation of that binary and connection of FX3 device during reboot i'm getting regular BSOD.

And driver tells the same - driver installation complete incorrectly.

0 Likes

Hello,

Please bind the FX3 device to the driver .inf file(path mentioned in the previous response) manually  from the device manager and check if you are facing the same problem.

Best Regards,

Yatheesh

0 Likes

Hello.

i removed all .inf files from windows/inf/oem*.inf and reinstalled driver again. After that driver installed correctly, FX3 chip is working.

Thank you, good luck

0 Likes