- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I complete a UVC camera with FX3 CyUSB3014 with guide of AN75779, but it works well in stream mode, but it goes bad in trigger mode;
The cmos sensor works in streaming mode, and outpus raw data; the raw data is transfered to PC through FX3 on USB bus. After I set this CMOS sensor into trigger mode, and have the trigger pin in high level, no transfer continues. the firmware prints log: "UVC: Completed 0 frames and 0 buffers".
I check the output of cmos sensor, PCLK,FV,and LV works well. it seems that the GPIF hasn't generate event to firmware, I don't know the reseaon, because the timing is good. In the meatime, I find, when the cmos sensor is in standby mode with trigger pin low, no PCLK,FV, and LV are found.
Solved! Go to Solution.
- Labels:
-
USB Superspeed Peripherals
- Tags:
- usb3014
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
Kindly confirm if you are referring to the trigger based still image capture.
Are you using AN75779 example firmware? Please mention the changes that you have made in the AN75779 firmware.
Can you please provide the timing diagram of Trigger signal, PCLK and FV, LV?
Best Regards
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content