Hi all,
I have FX3 firmware that combines AN75779 (modified to receive 32-bit GPIF data) and USB-to-serial. I'm using SuperSpeedKit connected to Zeadboard which sends 120fps 800x480 test pattern. I made all required changes in descriptors and both parts seems to work well except that UVC stream stucks after several seconds of video capture.
By "stucks" I mean that:
1) threads stop running so that I don't see "UVC: Completed ..." message anymore
2) If I use on-board debugger, debug session also stops responding at all
3) Capture software (Virtualdub/VLC) stop responding as no USB request are processed
Couple additional notes:
1) GPIF SM seems to continue to work because I toggle GPIO from GPIF callback and I can see it in scope.
2) ARM error handlers are not called (put there GPIO toggle also) so it's not CPU issue or memory leak
3) Suspend event not issued for no reason. I do LPM disable on UVC start and enable on UVC stop and return true in LPM CB exactly as in AN75779
Will greatly appreciate for any help
Solved! Go to Solution.
Hi Hemanth,
Thanks for patch. Now image is not corrupted although at least 2 frames were lost
Here is the output:
...
Frames done 49677. Limit reached 0 times
Frames done 49795. Limit reached 0 times
Frames done 49913. Limit reached 0 times
Frames done 50031. Limit reached 0 times
======== DMA Reset Event: Commit buffer failure (47) after frame 50132 ========
Frames done 50132. Limit reached 0 times
======== DMA Reset Event: Commit buffer failure (47) after frame 50135 ========
Frames done 50135. Limit reached 0 times
======== DMA Reset Event: Commit buffer failure (47) after frame 50135 ========
Frames done 50136. Limit reached 0 times
======== DMA Reset Event: Commit buffer failure (47) after frame 50136 ========
Frames done 50136. Limit reached 0 times
======== DMA Reset Event: Commit buffer failure (47) after frame 50136 ========
Frames done 50136. Limit reached 0 times
======== DMA Reset Event: Commit buffer failure (47) after frame 50136 ========
Frames done 50136. Limit reached 0 times
======== DMA Reset Event: Commit buffer failure (47) ad 0 times
======== DMA Reset Event: Commit buffer failure (47) after frame 50136 ========
Frames done 50136. Limit reached 0 times
======== DMA Reset Event: Commit buffer failure (47) after frame 50136 ========
Frames done 50136. Limit reached 0 times
======== DMA Reset Event: Commit buffer failure (47) after frame 50136 ========
Frames done 50136. Limit reached 0 times
======== DMA Reset Event: Commit buffer failure (47) after frame 50136 ========
Frames done 50136. Limit reached 0 times
======== DMA Reset Event: Commit buffer failure (47) after frame 50136 ========
Frames done 50136. Limit reached 0 times
======== DMA Reset Event: Commit buffer failure (47) after frame 50136 ========
Frames done 50136. Limit reached 0 times
======== DMA Reset Event: Commit buffer failure (47) after frame 50136 ========
Frames done 50136. Limit reached 0 times
======== DMA Reset Event: Commit buffer failure (47) after frame 50136 ========
Frames done 50136. Limit reached 0 times
======== DMA Reset Evs done 50136. Limit reached 0 times
======== DMA Reset Event: Commit buffer failure (47) after frame 50136 ========
Frames done 50136. Limit reached 0 times
======== DMA Reset Event: Commit buffer failure (47) after frame 50136 ========
Frames done 50136. Limit reached 0 times
======== DMA Reset Event: Commit buffer failure (47) after frame 50136 ========
Frames done 50136. Limit reached 0 times
======== DMA Reset Event: Commit buffer failure (47) after frame 50136 ========
Frames done 50136. Limit reached 0 times
======== DMA Reset Event: Commit buffer failure (47) after frame 50136 ========
Frames done 50136. Limit reached 0 times
======== DMA Reset Event: Commit buffer failure (47) after frame 50136 ========
Frames done 50136. Limit reached 0 times
Frames done 50253. Limit reached 0 times
Frames done 50371. Limit reached 0 times
Frames done 50489. Limit reached 0 times
Frames done 50607. Limit reached 0 times
...
Best regards,
Leonid
Hi Hemanth,
Now it stops by itself:
Frames done 50974. Limit reached 0 times
Frames done 51092. Limit reached 0 times
Frames done 51210. Limit reached 0 times
Frames done 51328. Limit reached 0 times
Frames done 51446. Limit reached 0 times
Frames done 51564. Limit reached 0 times
======== DMA Reset Event: Commit buffer failure (0) after frame 51658 ========
*** CyFxUVCApplnStop ***
Total 51658 frames
Best regards,
Leonid
Hi Hemanth,
Thanks for patch. Now image is not corrupted although at least 2 frames were lost
Here is the output:
...
Frames done 49677. Limit reached 0 times
Frames done 49795. Limit reached 0 times
Frames done 49913. Limit reached 0 times
Frames done 50031. Limit reached 0 times
======== DMA Reset Event: Commit buffer failure (47) after frame 50132 ========
Frames done 50132. Limit reached 0 times
======== DMA Reset Event: Commit buffer failure (47) after frame 50135 ========
Frames done 50135. Limit reached 0 times
======== DMA Reset Event: Commit buffer failure (47) after frame 50135 ========
Frames done 50136. Limit reached 0 times
======== DMA Reset Event: Commit buffer failure (47) after frame 50136 ========
Frames done 50136. Limit reached 0 times
======== DMA Reset Event: Commit buffer failure (47) after frame 50136 ========
Frames done 50136. Limit reached 0 times
======== DMA Reset Event: Commit buffer failure (47) after frame 50136 ========
Frames done 50136. Limit reached 0 times
======== DMA Reset Event: Commit buffer failure (47) ad 0 times
======== DMA Reset Event: Commit buffer failure (47) after frame 50136 ========
Frames done 50136. Limit reached 0 times
======== DMA Reset Event: Commit buffer failure (47) after frame 50136 ========
Frames done 50136. Limit reached 0 times
======== DMA Reset Event: Commit buffer failure (47) after frame 50136 ========
Frames done 50136. Limit reached 0 times
======== DMA Reset Event: Commit buffer failure (47) after frame 50136 ========
Frames done 50136. Limit reached 0 times
======== DMA Reset Event: Commit buffer failure (47) after frame 50136 ========
Frames done 50136. Limit reached 0 times
======== DMA Reset Event: Commit buffer failure (47) after frame 50136 ========
Frames done 50136. Limit reached 0 times
======== DMA Reset Event: Commit buffer failure (47) after frame 50136 ========
Frames done 50136. Limit reached 0 times
======== DMA Reset Event: Commit buffer failure (47) after frame 50136 ========
Frames done 50136. Limit reached 0 times
======== DMA Reset Evs done 50136. Limit reached 0 times
======== DMA Reset Event: Commit buffer failure (47) after frame 50136 ========
Frames done 50136. Limit reached 0 times
======== DMA Reset Event: Commit buffer failure (47) after frame 50136 ========
Frames done 50136. Limit reached 0 times
======== DMA Reset Event: Commit buffer failure (47) after frame 50136 ========
Frames done 50136. Limit reached 0 times
======== DMA Reset Event: Commit buffer failure (47) after frame 50136 ========
Frames done 50136. Limit reached 0 times
======== DMA Reset Event: Commit buffer failure (47) after frame 50136 ========
Frames done 50136. Limit reached 0 times
======== DMA Reset Event: Commit buffer failure (47) after frame 50136 ========
Frames done 50136. Limit reached 0 times
Frames done 50253. Limit reached 0 times
Frames done 50371. Limit reached 0 times
Frames done 50489. Limit reached 0 times
Frames done 50607. Limit reached 0 times
...
Best regards,
Leonid
Hi Leonid,
Yes. Loss of few frames while handling the commit buffer failure is unavoidable.
Regards,
Hemanth
Hi Hemanth,
Frame loss and on 30 fps for such low resolution as 800x482 must be considered as major issue for Cypress.
Meanwhile I'm thinking about some workaround for this issue. So far my idea is to use auto DMA instead of manual. To do so I need to provide UVC header in hardware for each buffer (16368 bytes).
If you think it's feasible, could you please mention required steps I need to do in order to switch to auto DMA?
Anyway, I would like to arrange a real time discussion (phone/skype/zoom/teams/ etc..) with you or your colleagues about this issue.
Best regards,
Leonid
During streaming, if there is enough delay from the Host in taking data from FX3, then there can be a case where DMA buffers allocated to video channel are overflowed with the frame data. In such scenarios flow control can be tried on the GPIF interface - so that FPGA holds the data during this delay. If the delay is large enough such that FPGA also runs out of memory to store the data, then few frames will be lost.