- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi, Sir
I use fx3 as the uvc device, but after working for a while, the image will be abnormal.
Does anyone know how to fix it?
Thank you very much.
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
1. Change the CY_FX_UVC_STREAM_BUF_SIZE, CX3_UVC_STREAM_BUF_COUNT; in dmaMulti Channel configuration to 0x8FD0, 3 respectively.
2. Set the Counters DATA and ADDR_COUNTERS in GPIF state machine by following this formula = (36816/ GPIF Bus Width) - 1
3. Change the following line in the probe control settings:
i.e No. of bytes device can receive in single payload.
0x00, 0x90, 0x00, 0x00 /* No. of bytes device can rx in single payload: 36KB */
4. Do the above three modifications and build the firmware then check the debug prints.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Share the following details to debug this issue.
1. Enable the DEBUG Prints in the firmware. Check whether there is any commit buffer failures
2. What is the operating system? Windows, Linux or Mac?
3. What is the resolution and format?
4. What is the sensor?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi srdr
Thank you for your reply.
1. Sorry, I'm not familiar with FX3.The example I use is AN75779.How to enable debug printing function?
2. Use on Windows.
3. 1920*1080 20fps, YUV422 format, Pixel Clock 96MHz.
4. ONSEMI AR0231+AP0202
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello Eden Wu,
- The AN75779 has got UART debug prints. Kindly, collect the UART logs and share the same. In case you are using the FX3 SuperSpeed Explorer Kit, the board has got an on board USB-Serial converter. This can be used to convert to UART data onto USB and viewed on the standard terminals on the host (like TeraTerm).
- Also, mention the buffer size and count that has been used.
Best regards,
Srinath S
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Srinath S
I got a error code:
Error in CyU3PDmaMultiChannelCommitBuffer: code 71
Can you tell me how to fix this issue?
Thank you very much~
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
1. Change the CY_FX_UVC_STREAM_BUF_SIZE, CX3_UVC_STREAM_BUF_COUNT; in dmaMulti Channel configuration to 0x8FD0, 3 respectively.
2. Set the Counters DATA and ADDR_COUNTERS in GPIF state machine by following this formula = (36816/ GPIF Bus Width) - 1
3. Change the following line in the probe control settings:
i.e No. of bytes device can receive in single payload.
0x00, 0x90, 0x00, 0x00 /* No. of bytes device can rx in single payload: 36KB */
4. Do the above three modifications and build the firmware then check the debug prints.