FX3 USB Connector/Header options

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Hi,

   

I working on a FX3 board layout with USB3 functionality. The product relies on high speed USB3 data transfers. I was wonder if instead of using a USB A/C type connectors, if I can just use a 9 pin header (1.27mm pitch or 2.54mm pitch) and just solder a usb 3 cable to it

   

1) Will this work?

   

2) if yes, will there be any transfer speed limitations?

   

 

   

Can I use a FFC (Flat flexible cable) connector as another option? Are there any design requirements that I should keep in mind when using such a connector for USB3 communication rather than a typical USB 3 A/B/C connector?

   

 

   

The point is to have a USB cable attached to the board directly instead of a connector.

   

 

   

Any help will be appreciated.

   

Thanks

   

Mak

0 Likes
2 Replies
Anonymous
Not applicable

We do not recommend you have headers for USB3 connections.  

   

However, we have seen people using Flex cable for similar implementation. 

0 Likes
Anonymous
Not applicable

Thank you!

0 Likes