No I have the FX3 DVK board connected to our FPGA board and try to set up the sync slave FIFO connetion. If I send data from host to the OUT EP, the FX3 delivers 2 additional words before the transmitted data. How can I setup the FX3 correctly to avoid this? I set up the endpoints and sockets in this way:
#define CY_FX_EP_PRODUCER 0x06 /* EP 6 OUT */
#define CY_FX_EP_CONSUMER 0x82 /* EP 2 IN */
#define CY_FX_EP_PRODUCER_USB_SOCKET 0x06 /* USB Socket 6 is producer */
#define CY_FX_EP_CONSUMER_USB_SOCKET 0x02 /* USB Socket 2 is consumer */
/* Used on FX3 silicon. */
#define CY_FX_EP_PRODUCER_PPORT_SOCKET CY_U3P_PIB_SOCKET_0 /* P-port Socket 0 is producer */
#define CY_FX_EP_CONSUMER_PPORT_SOCKET CY_U3P_PIB_SOCKET_1 /* P-port Socket 1 is consumer */
And set up the GPIF II to connect the flags fixed to the threads:
{CY_U3P_PIB_GPIF_CTRL_BUS_SELECT_ADDRESS(4) , 0x00000011}, //FLAGA = Fixed to Thread 1
{CY_U3P_PIB_GPIF_CTRL_BUS_SELECT_ADDRESS(5) , 0x00000010}, //FLAGB = Fixed to Thread 0
This works well, but there are 2 cycles with 0x0000 data in the FIFO. Do I have to use the partial flags with watermark value? Is yes, how to configure?
Attached you can find the ChipScope output for this beha
Argh, some errors:
the last word schould be "behavior"
I sent only the words 0x1111, 0x2222, 0x3333, 0x4444 and 0x8000 to the OUT EP.
There is 2 clock cycles' delay once fx3 enters "output" mode.