- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
I setup fx3 superspeed kit with FPGA board to test streamOUT example provided. Streamer and loopback functions well. I can transmit data and receive back. I am trying to transmit 302700 bytes of data or 302700/4=76800 counts of 32 bits. It seems to stop at counter 3072. Counter goes from 76800 to 0 (76799 to 0 to be exact). I am using 32 bits width bus. So each count is 32 bits. So 294912 bytes of data seems to be transmitted just normal, until it stops abnormally. Is there any maximum size limit on Control Center software?
It has a burst size of 4096*4=16384 bytes per transfer. Since 76800-72704 = 4096 and data stops and starts again. It seems to work just fine, between bursts, until it hits 3072 count, where FX3 control center side seems to do nothing.
Solved! Go to Solution.
- Labels:
-
USB Superspeed Peripherals
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
If streamer and bulkloop examples are working fine with the Cyclone V starter boards, I dont think there would be any changes to be made based on the FPGA.
In the Control Center software could you try sending a Zero length packet after sending 307200 bytes and let us know if the data is sent out properly?
Best Regards,
AliAsgar
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
Please let us know if you have made any modifications to the firmware shared with AN65974.
In default firmware, if STREAM_IN_OUT is enabled, the burst length will be 16. Also, confirm if the FPGA code is similar to the one shared with AN65974.
Rashi
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
Hello,
Is there any update on this issue? I have tried with default FPGA code and still have the issue.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
In the UtoP DMA callback of the FX3 firmware, increment a counter during a PROD event and increment another counter during a CONS event. Make sure that the PROD and CONS notifications are enabled for the DMA channel.
Print these counter values in the for (;;) loop and share with us the UART debug logs.
When the issue occurs, what error is seen on the Control Center software?
Please enable the STREAM_IN_OUT macro in the firmware to enable burst transfers.
Best Regards,
AliAsgar
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
This is the debug print when I try to send 307200 bytes.
This is when I try to send 2500 bytes.
Control Center software doesn't show any errors or issues. It even shows last address 4AFF0 with all the correct data. But apparently there is CYU3P_PIB_ERR_THR3_RD_UNDERRUN▒▒CYU3P_PIB_ERR_THR3_RD_UNDERRUN error.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
Could you try to send a Zero length packet after sending 302700 bytes and check if the issue is still occurring?
Also please try to read data from FX3 based on the flag status. Please refer to AN65964 application note for details on cycle latency between RD signal and Flag. Not having proper flow control between FX3 and FPGA leads to UNDERRUN error. Make sure the timing specs are met according to AN65974.
Best Regards,
AliAsgar
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
The thing is streamer and boolkloop examples work without issues. I am using default projects for FPGA board and FX3 superspeed kit with HSMC connector. Although, instead of Cyclone III starter board used in example AN65974, I am using Cyclone V starter board. Does that mean default projects with RD signal and flags need to be adjusted to specific board?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
If streamer and bulkloop examples are working fine with the Cyclone V starter boards, I dont think there would be any changes to be made based on the FPGA.
In the Control Center software could you try sending a Zero length packet after sending 307200 bytes and let us know if the data is sent out properly?
Best Regards,
AliAsgar