- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
FX3 Serial number in Bootloader mode (j4 jumper insert - PMODE)
Hi,
I'm using multiple FX3 board devices and I connect them under 4 DS port HUB,
When I restart the computer all off them starting with Yellow Exclamation Mark Issue in Device Manager.
I think it's because when all of the FX3 in Bootloader mode then the Serial number is the same
Serial number "USB\VID_04B4&PID_00F3\0000000004BE"
Can I change the serial number of the Bootloader mode? I now how to change the descriptor serial number of the firmware that I'm burning to the device but I don’t know how to change the descriptor serial number when the device is in Bootloader mode.
I add picture so you can see the problem inside the device manager.
You can reproduce the problem at your end by:
- Connecting 4 FX3 with J4 jumper insert under HUB
- Restart the pc
- Enter to device manger to see if the device enumerate proper
Thanks,
EliW.
Solved! Go to Solution.
- Labels:
-
USB Superspeed Peripherals