Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

USB superspeed peripherals Forum Discussions

NoAr_1540581
Level 5
Level 5
250 sign-ins 100 replies posted 100 sign-ins

Hello

I'm referring to the FX3 datasheet reset sequence Figure 29
Please tell me if the following understanding is correct
#1. Is it correct to understand that the power supply stabilization time before releasing the H/W reset is tRPW = 1ms (Min)?
#2. Is it correct to understand that the clock stabilization time before releasing the H/W reset is tRPW = 1ms (Min)?

#3. Assuming SPI boot, the sequence after H/W reset release is recognized as follows.
Correct?
 After H / W reset release → PLL lock start → PLL lock complete → IC internal reset release → SPI access start (boot image load start)
Please let us know, if tere are some misunderstanding mentioned above.

Best Regards

Arai

0 Likes
1 Solution
Rashi_Vatsa
Moderator
Moderator
Moderator
5 likes given 500 solutions authored 1000 replies posted

Hello Arai san,

#1. Is it correct to understand that the power supply stabilization time before releasing the H/W reset is tRPW = 1ms (Min)?

>>  Yes. Please refer to KBA Power Up Sequence for FX3 – KBA221826 - Cypress Developer Community  If the Power supply take more time to stabilize than the reset time can be more than 1ms but the minimum time for reset should be 1 ms

2. Is it correct to understand that the clock stabilization time before releasing the H/W reset is tRPW = 1ms (Min)?

>> Yes, as per figure 29 of FX3 datasheet the clock should be stable before releasing the RESET# (RESET - HIGH)

#3. Assuming SPI boot, the sequence after H/W reset release is recognized as follows.
Correct?
 After H / W reset release → PLL lock start → PLL lock complete → IC internal reset release → SPI access start (boot image load start)

>>  If the minimum reset time is met and clock and all power supplies are stable then the bootloader will start firmware download after tRR time.

Regards,
Rashi

View solution in original post

0 Likes
1 Reply
Rashi_Vatsa
Moderator
Moderator
Moderator
5 likes given 500 solutions authored 1000 replies posted

Hello Arai san,

#1. Is it correct to understand that the power supply stabilization time before releasing the H/W reset is tRPW = 1ms (Min)?

>>  Yes. Please refer to KBA Power Up Sequence for FX3 – KBA221826 - Cypress Developer Community  If the Power supply take more time to stabilize than the reset time can be more than 1ms but the minimum time for reset should be 1 ms

2. Is it correct to understand that the clock stabilization time before releasing the H/W reset is tRPW = 1ms (Min)?

>> Yes, as per figure 29 of FX3 datasheet the clock should be stable before releasing the RESET# (RESET - HIGH)

#3. Assuming SPI boot, the sequence after H/W reset release is recognized as follows.
Correct?
 After H / W reset release → PLL lock start → PLL lock complete → IC internal reset release → SPI access start (boot image load start)

>>  If the minimum reset time is met and clock and all power supplies are stable then the bootloader will start firmware download after tRR time.

Regards,
Rashi
0 Likes
This widget could not be displayed.