- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
is it possible to store image data in the sdcard through streamin mode from the fpga?
my hardware design is..
gpif 2 (slavefifo) (ptos & stou) usb2/3
image sensor<->fpga<-------------------------> fx3 sdcard port <---------------> pc in slavefifo mode and without any filesystems in the firmware i.e. only raw data streaming.
ptos ->p port data to s port (sdcard write operation).
stou ->s port data to u port(sdcard read operation).
regards,
geetha.
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Geetha,
Yes it is possible to store data from GPIF side to SD card using a file system in the firmware side. Please look into "fatfs" firmware that comes along with FX3 SDK. Then to read the data from the host there is no need to implement file system on the firmware side. Your device should come up as a mass storage device and then window driver will take care of the file operations on the SD card.
Thanks & Regards
Abhinav