Announcements

Learn how to optimise USB-C for your designs at 18 May's USB-C PD Webinar.
Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

lock attach
Attachments are accessible only for community members.
noah
Level 1
Level 1
5 sign-ins First reply posted First question asked

Hi I am noah

I am working with FX3 evaluation board for UVC application

My latest work was 1920x1080 30Hz UVC yuv2 video, It works well

But I need 1920x1080 60Hz UVC application

I modified from example application (an75779)

I changed 32-bit Data bus, resolution, frame rate, buffer count in source code

in GPIF design, data_count, address_count set to 4091

But, video is broken

I don't know what I miss

Please check my attached project

I am using vitualDub, and it recognize well 1920x1080 60hz video but screen is broken

my question is that fx3 works well for 1920x1080 60hz uvc??

thank you

4 Replies
AliAsgar
Moderator
Moderator
Moderator
1000 replies posted 250 solutions authored 750 replies posted

Hi Noah,

Could you let us know the value of PCLK?

Also enable debug prints for the firmware and kindly share the debug prints with us.

Best Regards,
AliAsgar

0 Likes
noah
Level 1
Level 1
5 sign-ins First reply posted First question asked

Hi AliAsgar

PCLK is 74.25Mhz 

horizontal sync total 1100 clock, vertical sync total 1125 clock

1125 x 1100 x 60Hz x (1/74.25Mhz) = 1 sec,  is it right?

If you need to see debug print log, I will prepare log file, It need more time

Do not have any problem in my source code?

thank you for your fast response

 

0 Likes
lock attach
Attachments are accessible only for community members.
noah
Level 1
Level 1
5 sign-ins First reply posted First question asked

Hi AliAsgar

I attach debug print log, source code

this message repeated, "DMA Reset Event : Commit buffer failure "

I checked uvc video using vitual dub 1.10.4(64-bit) on windows 10

I did resize dma buffer 16KB -> 32KB, But it was useless. same error message is occurred

Please give me help

thank you

0 Likes
lock attach
Attachments are accessible only for community members.
AliAsgar
Moderator
Moderator
Moderator
1000 replies posted 250 solutions authored 750 replies posted

Hi Noah,

1. Please find the attached firmware project, which is modified to print the frame size.
2. Could you check if the same issue is seen on different Host Applications and/or different Host PCs?

Best Regards.
AliAsgar

0 Likes