Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

USB superspeed peripherals Forum Discussions

ShYu_2612661
Level 1
Level 1
First reply posted First question asked First like given

Hi, I plan to interface a python 500 Cmos camera with Cypress EZ-USB FX3. The frame rate of the camera is 500 fps(Pixels:600*800). So I'm just wondering to know if it is possible to achieve 500 fps?

Many thanks,

Frank

0 Likes
1 Solution
Rashi_Vatsa
Moderator
Moderator
Moderator
5 likes given 500 solutions authored 1000 replies posted

Hi Frank,

The GPIF II interface can run at a maximum of 100MHz, with a maximum 32-bit data bus. The maximum throughput supported by the GPIF interface is 32 bits * 100MHz = 3.2Gbps (400MBps).

The data coming from the sensor should be less than or equal to maximum throughput supported by GPIF interface (400MBps) i.e.

600*800*bytes/pixel* 500 < = 400MBps

When GPIF bus width is 32 bits and PCLK is 100 MHz, if Bytes/pixel = 1, then 600*800*1*500 < 400 MBps

Note: 3.2Gbps throughput is for the case when GPIF bus width is 32 bits and 100 MHz clock. At PCLK 100MHz, configuring the GPIF interface for 8/16/24 bits bus width will reduce the data throughput.

Please let me know if any queries on this.

Regards,

Rashi

Regards,
Rashi

View solution in original post

2 Replies
Rashi_Vatsa
Moderator
Moderator
Moderator
5 likes given 500 solutions authored 1000 replies posted

Hi Frank,

The GPIF II interface can run at a maximum of 100MHz, with a maximum 32-bit data bus. The maximum throughput supported by the GPIF interface is 32 bits * 100MHz = 3.2Gbps (400MBps).

The data coming from the sensor should be less than or equal to maximum throughput supported by GPIF interface (400MBps) i.e.

600*800*bytes/pixel* 500 < = 400MBps

When GPIF bus width is 32 bits and PCLK is 100 MHz, if Bytes/pixel = 1, then 600*800*1*500 < 400 MBps

Note: 3.2Gbps throughput is for the case when GPIF bus width is 32 bits and 100 MHz clock. At PCLK 100MHz, configuring the GPIF interface for 8/16/24 bits bus width will reduce the data throughput.

Please let me know if any queries on this.

Regards,

Rashi

Regards,
Rashi

Thanks Rashi,

This solves my question

Cheers,

Frank

0 Likes