In EZ-USB FX 3, a crystal is inserted between the XTALIN pin and the XTALOUT pin
It can be connected, or an external clock can be connected to the CLKIN pin
Although it is described in the data sheet, when connecting to XTALIN / OUT
Is it OK to connect the CLK IN terminal?
Solved! Go to Solution.
Hello,
The FX3 chooses the input clock based on the FSLC[2:0] pins. Although crystal and clock are connected, FX3 chooses one of those based on the FSLC[2:0] pin strap connection.
Best regards,
Srinath S
Hello,
The FX3 chooses the input clock based on the FSLC[2:0] pins. Although crystal and clock are connected, FX3 chooses one of those based on the FSLC[2:0] pin strap connection.
Best regards,
Srinath S
thank you for your answer.
As contents that I wanted to check
When input of XTAL IN is selected
Which of the following processes is correct for pin processing of CLK IN
※ PullUp or Pulldown or OPNEN
Hello,
When you are using XTALIN input, the CLKIN pin can be left floating (unconnected).
Best regards,
Srinath S
Thank you for your early reply.
I understand that it can be unconnected
Also, if there is a machine thank you for your consideration.
Hello,
Sorry if I had misunderstood your previous question. Can you please let me know what you mean by "machine"?
Best regards,
Srinath S
Is it about the use of machines that use devices?
There is content that you want me to check by adding 1 point
As a terminal for CYUSB 3014-BZXIT boot option
Below, when not using the function Which processing will be the terminal processing
※ Pullup or Pulldown or OPEN
· FX 3 boot option I 2 C
⇒ I2C_GPIO [58/59]
· FX 3 Boot Option SPI
⇒ GPIO [53/54/55/56]
· JTAG
⇒ TCK / TMS / TRST # / TDO / TDI
Hello,
- I2C lines need to be added with a pull up resistor recommended value being 2kohm.
- SPI lines and JTAG lines do not need a pull-up or pull-down resistor and can be left open.
Best regards,
Srinath S
OK. Thank you for your reply.