Tip / ログイン to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
ManabuIto
Level 1
Level 1
First question asked Welcome!

FX3で開発を行っています。
これを製品化する場合、VendorIDの取得以外に商用利用条件は何かありますか?

ーーーーーーーーーーーーーーーー

We are developing with FX3.
When commercializing this, are there any commercial terms of use other than obtaining a Vendor ID?

0 件の賞賛
1 解決策
Rashi_Vatsa
Moderator
Moderator
Moderator
5 likes given 500 solutions authored 1000 replies posted

Hello,

Please refer to the license folder of the FX3 SDK (Path: SDK Installation Path\Cypress\EZ-USB FX3 SDK\1.3\license)

- Please refer to this KBA  License for FX3 SDK - KBA222519 - Cypress Developer Community  

If cyusb3.sys driver is used for product (for production/distribution) with custom VID/PID, then customer should not use any of the pre-existing Cypress VID/PID in their modified INF apart from the device (like FX2 , FX3) Bootloader VID/PID.

Please refer to this thread  Solved: What am i allowed to do with default PID/VID - Cypress Developer Community  

Regards,
Rashi

元の投稿で解決策を見る

0 件の賞賛
1 返信
Rashi_Vatsa
Moderator
Moderator
Moderator
5 likes given 500 solutions authored 1000 replies posted

Hello,

Please refer to the license folder of the FX3 SDK (Path: SDK Installation Path\Cypress\EZ-USB FX3 SDK\1.3\license)

- Please refer to this KBA  License for FX3 SDK - KBA222519 - Cypress Developer Community  

If cyusb3.sys driver is used for product (for production/distribution) with custom VID/PID, then customer should not use any of the pre-existing Cypress VID/PID in their modified INF apart from the device (like FX2 , FX3) Bootloader VID/PID.

Please refer to this thread  Solved: What am i allowed to do with default PID/VID - Cypress Developer Community  

Regards,
Rashi
0 件の賞賛