- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi , I need to Download the Firmware into SPI flash without switching the Fx3 into boot mode using jumper.
Is it possible ??
If Yes, then from where I get the reference .cpp Application code ?
Is "cyfxflashprog" Example Firmware works in that case ?
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
For this, your device should have a vendor interface and should also support the vendor commands that are present in the cyfxflashprog example project for programming the SPI flash. After this you need to develop a host application that sends these vendor commands to the device. You can make use of the following source code as a reference for building the utility:
C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\application\cpp\fwdownload_fx3
Jayakrishna
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
For this, your device should have a vendor interface and should also support the vendor commands that are present in the cyfxflashprog example project for programming the SPI flash. After this you need to develop a host application that sends these vendor commands to the device. You can make use of the following source code as a reference for building the utility:
C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\application\cpp\fwdownload_fx3
Jayakrishna
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Can we read spi Flash when the FX3 Bootloader is running?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
I did not properly understand this question. Are you talking about the ROM bootloader? If yes, then we do not have any control on the ROM bootloader. So, we cannot read the SPI flash when it is running.
Jayakrishna
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
In S25FL127SABMFI101 SPI Flash what is the 1) number of sector ?
2) Sector Size ?
3) Number of Page ?
4) Page Size ?
Need to Write Firmware into the Flash memory . I am reference the UsbSpiDmaMode Firmware Example code.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
Please refer to the datasheet of the flash part to understand the details. If there are further queries, then please create a new thread in our flash community and one of our engineers will answer them.
Jayakrishna