Announcements

Ever wondered how you could apply Infineon products in a sustainable way? Join us at OktoberTech Asia Pacific and get inspired Click here to register for FREE.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

USB superspeed peripherals Forum Discussions

ankitvats846
Level 2
10 replies posted 10 sign-ins 5 questions asked
Level 2

Hi , I need to Download the Firmware into SPI flash without switching the Fx3 into boot mode using jumper.

Is it possible ??

If Yes, then from where  I get the reference  .cpp Application code ?

Is  "cyfxflashprog" Example Firmware works in that case ? 

0 Likes
1 Solution
JayakrishnaT_76
Moderator
Moderator First question asked 1000 replies posted 750 replies posted
Moderator

Hello,

For this, your device should have a vendor interface and should also support the vendor commands that are present in the cyfxflashprog example project for programming the SPI flash. After this you need to develop a host application that sends these vendor commands to the device. You can make use of the following source code as a reference for building the utility:

C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\application\cpp\fwdownload_fx3

Best Regards,
Jayakrishna

View solution in original post

5 Replies
JayakrishnaT_76
Moderator
Moderator First question asked 1000 replies posted 750 replies posted
Moderator

Hello,

For this, your device should have a vendor interface and should also support the vendor commands that are present in the cyfxflashprog example project for programming the SPI flash. After this you need to develop a host application that sends these vendor commands to the device. You can make use of the following source code as a reference for building the utility:

C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\application\cpp\fwdownload_fx3

Best Regards,
Jayakrishna
ankitvats846
Level 2
10 replies posted 10 sign-ins 5 questions asked
Level 2

Can we read spi Flash when the FX3 Bootloader is running? 

 

0 Likes
JayakrishnaT_76
Moderator
Moderator First question asked 1000 replies posted 750 replies posted
Moderator

Hello,

I did not properly understand this question. Are you talking about the ROM bootloader? If yes, then we do not have any control on the ROM bootloader. So, we cannot read the SPI flash when it is running.

Best Regards,
Jayakrishna
0 Likes
ankitvats846
Level 2
10 replies posted 10 sign-ins 5 questions asked
Level 2

Hi, 

In S25FL127SABMFI101 SPI Flash what is the   1) number of sector ?

                                                                                                2) Sector Size ?

                                                                                                 3)  Number of Page ?

                                                                                                 4) Page Size ? 

Need to Write Firmware  into the Flash memory . I am reference the UsbSpiDmaMode Firmware Example code.

 

0 Likes
JayakrishnaT_76
Moderator
Moderator First question asked 1000 replies posted 750 replies posted
Moderator

Hello,

Please refer to the datasheet of the flash part to understand the details. If there are further queries, then please create a new thread in our flash community and one of our engineers will answer them.

Best Regards,
Jayakrishna
0 Likes