Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

USB superspeed peripherals Forum Discussions

Anonymous
Not applicable

Hi, 

   

I am working on a project with FX3 trying to obtain live video at 240 fps with resolution 640 x 120 using image sensor MT9V034. 

   

I have checked the bandwidth of FX3 (5Gbps), UVC (128Mbps for USB3.0) and the image sensor (27Mbps) and they all support the frame rates at this resolution (640 x 120 x 1 x 240 = 18.43Mbps since the sensor output is monochrome). 

   

I am wondering does this mean the whole system can work properly at 240 fps?

   

Best,

   

Eric

0 Likes
1 Reply
Anonymous
Not applicable

Hi Eric,

   

It is feasible to stream 640*120 @ 240fps video through FX3.

0 Likes