Sep 14, 2020
04:00 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Sep 14, 2020
04:00 AM
Hello,
I designed a camera that the video stream runs on a UVC driver and the command interface on the control channel uses the Cypress fx3 example device 1 driver (I used the guide to install it).
It works well in win7 and win 10 but I can't find the Cypress fx3 example device 1 driver for linux.
I use the latest release of Ubuntu.
This is the results for: cyusb.conf and lsusb -t:
Where can I find the driver?
All the best,
Ofer.
Solved! Go to Solution.
1 Solution
Attachments are accessible only for community members.
Sep 15, 2020
06:16 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Sep 15, 2020
06:16 AM
Hello,
Please try adding the VID, PID and custom string entry as Cypress FX3 Example device 1 and 2 in the cyusb.conf file and try using the library.
You can also replace the attached cyusb.conf file in the linux SDK, in which the two entries are added.
Thanks,
Yatheesh
6 Replies