Hello,
We want to use CyU3PMipicsiSetSensorControl(CY_U3P_CSI_IO_XRES,CyTrue); in the BootLedBlink example main.c line 83.
We attached also the source code .The result when compile is:
*** Incremental Build of configuration Debug for project BootLedBlink ****
cs-make all
'Building target: BootLedBlink.elf'
'Invoking: Cross ARM C Linker'
arm-none-eabi-gcc -mcpu=arm926ej-s -marm -mthumb-interwork -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections -Wall -g3 -T "C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\/fw_build/boot_fw/cyfx3.ld" -nostartfiles -Xlinker --gc-sections -L"C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\/boot_lib/1_3_3/lib" -L"C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\/fw_lib/1_3_3/fx3_debug" -L"C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\ARM GCC\/lib/gcc/arm-none-eabi/4.8.1" -L"C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\ARM GCC\/arm-none-eabi/lib" -Wl,-Map,"BootLedBlink.map" -Wl,-d -Wl,-elf -Wl,--no-wchar-size-warning -Wl,--entry,Reset_Handler -o "BootLedBlink.elf" ./I2C.o ./cyfx_gcc_startup.o ./main.o -lcyfx3boot -lcyu3mipicsi -lc -lgcc
C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\/fw_lib/1_3_3/fx3_debug\libcyu3mipicsi.a(cyu3mipicsi.o): In function `CyU3PMipicsiRegisterRead':
cyu3mipicsi.c:(i.CyU3PMipicsiRegisterRead+0x54): undefined reference to `CyU3PI2cReceiveBytes'
cyu3mipicsi.c:(i.CyU3PMipicsiRegisterRead+0x68): undefined reference to `_tx_thread_sleep'
C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\/fw_lib/1_3_3/fx3_debug\libcyu3mipicsi.a(cyu3mipicsi.o): In function `CyU3PMipicsiRegisterWrite':
cyu3mipicsi.c:(i.CyU3PMipicsiRegisterWrite+0x50): undefined reference to `CyU3PI2cTransmitBytes'
cyu3mipicsi.c:(i.CyU3PMipicsiRegisterWrite+0x64): undefined reference to `_tx_thread_sleep'
C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\/fw_lib/1_3_3/fx3_debug\libcyu3mipicsi.a(cyu3mipicsi.o): In function `CyU3PMipicsiSetSensorControl':
cyu3mipicsi.c:(i.CyU3PMipicsiSetSensorControl+0xbc): undefined reference to `_tx_thread_sleep'
c:/program files (x86)/cypress/ez-usb fx3 sdk/1.3/arm gcc/bin/../lib/gcc/arm-none-eabi/4.8.1/../../../../arm-none-eabi/bin/ld.exe: BootLedBlink.elf: hidden symbol `CyU3PI2cReceiveBytes' isn't defined
c:/program files (x86)/cypress/ez-usb fx3 sdk/1.3/arm gcc/bin/../lib/gcc/arm-none-eabi/4.8.1/../../../../arm-none-eabi/bin/ld.exe: final link failed: Bad value
collect2.exe: error: ld returned 1 exit status
cs-make: *** [BootLedBlink.elf] Error 1
12:55:48 Build Finished (took 2s.213ms)
How can we use this function in bootledblink example?What do we have to include or to configure?
Thanks in advance!
Solved! Go to Solution.
Hello,
Please refer to this thread XRST pin on Low CYUSB306X and DS90UB960-Q1 deseria... - Cypress Developer Community