- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
We are trying to use the APIs CyU3PGpifWriteDataWords/CyU3PGpifReadDataWords using the FX3 as master and an FPGA as slave. The objective is to be able to write/read registers in the FPGA.
Note that the GPIF is set up for 32-bit synchronous with multiplexed data and address.
A simple example along with a minimal GPIF2 project would be very helpful. None of the examples in SDK 1.2.2 illustrate the use of the two APIs mentioned above.
Any help would be highly appreciated.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
We dont have an example project using CyU3PGpifWriteDataWords/CyU3PGpifRead APIs.
Please create a tech support case Support-> Technical Support -> Create a case, so that one of our engineers can guide you in this.
-PRJI
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
Please find the project that is attached to this post.
This one use the APIs CyU3PGpifWriteDataWords/CyU3PGpifReadDataWords.
I think the attached project meets your requirements.
Thanks,
sai krishna.
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
The example does not use multiplexed address and data bus and the API usage illustrated just writes data output.
In the absence of clear documentation, we have tried CyU3PGpifWriteDataWords/CyU3PGpifReadDataWords which seem to write data to the address associated with the thread index in multiplexed address/data mode. That is, the address is either 0,1,2,or 3.
How does one generate an arbitray address output? I need to be able to write to any arbitray 32-bit address in the external FPGA.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I have several followup up questions on this example code and other GPIF2.zip code in other threads,
The reason for the questions is that I need to parse 3 words of data from a control transaction and send them as a 3 Word GPIF transmit sequence to my FPGA. So during this transaction, I do not need DMA since I will parse the Setup commands and make a call to send the GPIF data manually.
First Question: If I understand the operation correctly, once the SW is up and running, the code is basically executing the infinite loop in “SlFifoAppThread_Entry”. Within this loop, once every second we transmit the FX3 sends a single word across the GPIF bus using the function call CyU3PGpifWriteDataWords (0, CyFalse, 1, &(tmp_data[tmp_cnt]), 0xFF); Is this correct?
Second Question: This has to do with setup of the DMA. Do we still need to configure all of the USB Producer/Consumer DMA items in CyFxSlFifoApplnStart (void) . If not, what is the minimum amount of configuration that I need do to just send data out the GPIF?
Third Question: How does the thread index and socket affect these “Manual” transactions?
Ken
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Now I try compile this project.
I get error:
Description Resource Path Location Type
conflicting types for 'CyU3PDmaBufferFree' cyfxtx.c /GPIF_Async line 476 C/C++ Problem
In file cyftx.c
May be a new compiler (I use USB suite 1.3.4)
How I can change build settings ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
And others:
Description Resource Path Location Type
undefined reference to `CyU3PUartInit' cyfxslfifoasync.c /SlaveFifoAsync line 107 C/C++ Problem
Description Resource Path Location Type
undefined reference to `CyU3PUartSetConfig' cyfxslfifoasync.c /SlaveFifoAsync line 124 C/C++ Problem
Description Resource Path Location Type
undefined reference to `CyU3PUartTxSetBlockXfer' cyfxslfifoasync.c /SlaveFifoAsync line 131 C/C++ Problem
But include files are presents:
#include "cyu3system.h"
#include "cyu3os.h"
#include "cyu3dma.h"
#include "cyu3error.h"
#include "cyu3usb.h"
#include "cyu3uart.h"
#include "cyfxslfifoasync.h"
#include "cyu3gpif.h"
#include "cyu3pib.h"
#include "pib_regs.h"