- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
import project “C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\firmware\dma_examples\cyfxbulklpmanual”, can not receive debug message in function CyFxBulkLpApplnInit(), I only change to another FW, host can receive debug message.
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
-If you are using the integrated debugger of the explorer board, pins (53:56) can be used for UART so if
- 16-bit configuration is used, the lpp mode should be UART_ONLY
- 32-bit configuration is used, the lpp mode should be DEFAULT
-If you want to use 16-bit configuration and DEFAULT lpp mode then pins (46:49) can be used for UART (this cannot use the integrated debugger)
Let me know which pins are you using for the UART and for which other firmware you are getting the debug prints.
Regards,
Rashi
Rashi
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
-If you are using the integrated debugger of the explorer board, pins (53:56) can be used for UART so if
- 16-bit configuration is used, the lpp mode should be UART_ONLY
- 32-bit configuration is used, the lpp mode should be DEFAULT
-If you want to use 16-bit configuration and DEFAULT lpp mode then pins (46:49) can be used for UART (this cannot use the integrated debugger)
Let me know which pins are you using for the UART and for which other firmware you are getting the debug prints.
Regards,
Rashi
Rashi
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I would like to add to my previous response that If you want to use integrated debugger of explorer board with 16-bit configuration and DEFAULT lpp mode then pins (46:49) should be shorted to pins (53:56).
Regards,
Rashi
Rashi