Hello everybody,
I'm using Qt Creator 7.0.1 based on Qt 6.2.3 (MVSC 2019, 64bits)
I got several issues while trying to build my project.
CyAPI.lib(CyAPI.obj):-1: erreur : LNK2019: symbole externe non r‚solu __imp_UnregisterDeviceNotification r‚f‚renc‚ dans la fonction "public: void __cdecl CCyUSBDevice::DestroyHandle(void)" (?DestroyHandle@CCyUSBDevice@@QEAAXXZ)
CyAPI.lib(CyAPI.obj):-1: erreur : LNK2019: symbole externe non r‚solu __imp_RegisterDeviceNotificationA r‚f‚renc‚ dans la fonction "private: bool __cdecl CCyUSBDevice::RegisterForPnpEvents(void *)" (?RegisterForPnpEvents@CCyUSBDevice@@AEAA_NPEAX@Z)
CyAPI.lib(CyAPI.obj):-1: erreur : LNK2019: symbole externe non r‚solu __imp_MessageBoxA r‚f‚renc‚ dans la fonction "int `public: bool __cdecl CCyUSBDevice::Open(unsigned char)'::`1'::catch$0" (?catch$0@?0??Open@CCyUSBDevice@@QEAA_NE@Z@4HA)
Do you know what is missing ?
my .pro file possess these libraries
LIBS += "C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\library\cpp\lib\x64\CyAPI.lib"
LIBS += "C:\Program Files (x86)\Windows Kits\10\Lib\10.0.19041.0\um\x64\SetupAPI.Lib"
LIBS += "C:\Program Files\Microsoft Visual Studio\2022\Community\VC\Tools\MSVC\14.31.31103\lib\x64\legacy_stdio_definitions.lib"
INCLUDEPATH += "C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\library\cpp\inc"
Solved! Go to Solution.
Hello Rashi_Vasta,
Thanks for your time and your answer.
I did exactly what you showed and I found the problem. The problem is that the user32.lib is not added by default in qt creator so I had to add it manually and it solved the issue.
Regards, Christophe
Hello,
The issue seems to be with linking the CYAPI.lib. Please check the linker settings as attached in the snippet.
Also, please confirm if the build configurations are same as the linker setting configuration
You can also refer to similar thread Solved: How do I integrate CyAPI.lib with Qt ? - Infineon Developer Community
Hello Rashi_Vasta,
Thanks for your time and your answer.
I did exactly what you showed and I found the problem. The problem is that the user32.lib is not added by default in qt creator so I had to add it manually and it solved the issue.
Regards, Christophe