Hi,
I am using a CX3 to bridge a MIPI camera to USB.
The CX3 is booting from SPI FLASH. There is no external I2C device connected.
In that case, do I still need the I2C pull-up resistors connected, or should it work without them?
The reason I ask is that my system works fine when I have the I2C resistors soldered in place (I see a live stream from the camera), but if I remove them, then the CX3 enumerates and appears in Device Manager, but I no longer see any images from the camera.
Thanks
Hugo
Solved! Go to Solution.
Hello Hugo,
It is necessary to have pull up resistors on I2C lines of CX3. This is because the MIPI CSI-2 block of CX3 is configured over I2C interface as mentioned in section 1.4 of CX3 TRM. The CX3 TRM comes along with FX3 SDK and can be found in the following location:
C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\doc\firmware
Hello Hugo,
It is necessary to have pull up resistors on I2C lines of CX3. This is because the MIPI CSI-2 block of CX3 is configured over I2C interface as mentioned in section 1.4 of CX3 TRM. The CX3 TRM comes along with FX3 SDK and can be found in the following location:
C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\doc\firmware
Hi, thanks for that.
Yes, I eventually discovered that in the TRM.
I do feel that, since the chip is literally useless without those resistors, it would have made sense to emphasise that strongly in the datasheet (or at least mention it).
Also, it would have been useful to have the option of internal pull-ups on those lines, since the other I/O pins have them.
Hugo
Editted
Dear Hugo,
We have already added the requirement of pull up resistors on I2C lines in CX3 datasheet. This can be found in Page 8 of CX3 datasheet. The snapshot of the same is attached below for your reference: