- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
We have purchased a CYUSB3KIT (FX3) development kit which we are planning to use for a video streaming application. My development environment is EZ USB suite and Intel NUC windows 7 64 bit. The development kit is not getting enumerated in device manager as well as in control centre. As per the jumper configurations mentioned in kit guide, pg 35 we made all connections still there is no change. The PMODE settings are SW25.1 and SW25.2 are off and SW25.3 and SW25.4 are off and J96,J97 are connected between 2-3 and J98 is left open for USB enumeration.
As of now, I have tried the following
- Modified jumper settings as per kit user guide
- Voltage levels were confirmed and VIO1 to VIO5 are giving 3.3V
- When powering via the external 5V DC jack, I have shorted J40,J47 and J53 connection is broken. Still there is no change
- Even after changing the cable provided along with the evaluation kit, there is no difference
- When trying to connect via an external Jlink Pro, target is getting detected and it measures 3.1V via GDB server, but connection fails
- As per instructions given in kit user guide, even tried running GDB debug configuration from Eclipse for ARM9, big endian, JTAG configuration. that stops session saying exception condition detected on fd0,error detected on stdin, quit (expect signal SIGINT when the program is resumed)
It would be great if you can help us in getting the board up and running.
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Annamol,
From the description my understanding is you are using CYUSB3KIT-001 (EZ-USB® FX3™ Development Kit (CYUSB3KIT-001) | Cypress Semiconductor )
What is the version of the KIT that you are using. This is available just next to J77 or below J96.
Your settings SW 25, J96, J97 and J98 settings looks fine.
What is the setting that have you used for SW9 (In buse power and external 5V DC)
I am not sure if you have to short J40 & J47.
Instead of external power when you bus power the device any of the LED's glow on the board such as (D14, D15, D16, D17 & D18)
Thank You & Regards,
Sudheer
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Annamol,
From the description my understanding is you are using CYUSB3KIT-001 (EZ-USB® FX3™ Development Kit (CYUSB3KIT-001) | Cypress Semiconductor )
What is the version of the KIT that you are using. This is available just next to J77 or below J96.
Your settings SW 25, J96, J97 and J98 settings looks fine.
What is the setting that have you used for SW9 (In buse power and external 5V DC)
I am not sure if you have to short J40 & J47.
Instead of external power when you bus power the device any of the LED's glow on the board such as (D14, D15, D16, D17 & D18)
Thank You & Regards,
Sudheer